Part Number: AM3358
Other Parts Discussed in Thread: AM3357, AM3356, , AM3359, AM3352
Hello -
I've been looking around the forum but couldn't find a direct answer to this question. According to this diagram (www.ti.com/.../datasheetdiagram.tsp, only the PRUs on the AM3357 and AM3359 can implement EtherCAT slave functionality. While it is clear that the AM3356 and AM3358 have the PRU subsystem as well, they are unable to implement EtherCAT slave. Is this due to a technical reason (e.g. the PRU subsystems are not the same across these 4 processors due to some technical/die limitation based on other included subsystems), or is it due to some sort of licensing/legal restriction artificially injected into the PRUs of the 3356/3358 at manufacture time just to prevent them from executing the EtherCAT PRU binary?
Thanks,
Darrin