Part Number: OMAPL138B-EP
Other Parts Discussed in Thread: OMAP-L138, DA8XX, PMP
Tool/software: Linux
Hi,
I am Using LCDK L138 . After Tftp Boot i got the Error as Follows.
NAND: 512 MiB
MMC: davinci: 0
Bad block table found at page 262080, version 0x01
Bad block table found at page 262016, version 0x01
In: serial
Out: serial
Err: serial
ARM Clock : 456000000 Hz
DDR Clock : 150000000 Hz
Net: Ethernet PHY: GENERIC @ 0x07
DaVinci-EMAC
Hit any key to stop autoboot: 0
BOOTP broadcast 1
DHCP client bound to address 192.168.1.13
Using DaVinci-EMAC device
TFTP from server 192.168.1.9; our IP address is 192.168.1.13
Filename 'uImage-omapl138-lcdk.bin'.
Load address: 0xc0700000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
##############
done
Bytes transferred = 2397856 (2496a0 hex)
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-3.3.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2397792 Bytes = 2.3 MiB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Booting Linux on physical CPU 0
Linux version 3.3.0 (gtbldadm@ubuntu-12) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 PREEMPT Tue Nov 5 20:19:32 EST 2013
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: AM18x/OMAP-L138 lcdk board
Memory policy: ECC disabled, Data cache writeback
BUG: mapping for 0x80000000 at 0xfffe0000 out of vmalloc space
DaVinci da850/omap-l138/am18x variant 0x1
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 32512
Kernel command line: console=ttyS2,115200n8 rw noinitrd root=/dev/nfs
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 128MB = 128MB total
Memory: 124860k/124860k available, 6212k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xc8800000 - 0xff000000 ( 872 MB)
lowmem : 0xc0000000 - 0xc8000000 ( 128 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.text : 0xc0008000 - 0xc0475000 (4532 kB)
.init : 0xc0475000 - 0xc049d000 ( 160 kB)
.data : 0xc049e000 - 0xc04cf760 ( 198 kB)
.bss : 0xc04cf784 - 0xc04eca6c ( 117 kB)
SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 227.32 BogoMIPS (lpj=1136640)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
Setting up static identity map for 0xc03625a0 - 0xc03625f8
gpiochip_add: registered GPIOs 0 to 31 on device: DaVinci
gpiochip_add: registered GPIOs 32 to 63 on device: DaVinci
gpiochip_add: registered GPIOs 64 to 95 on device: DaVinci
gpiochip_add: registered GPIOs 96 to 127 on device: DaVinci
gpiochip_add: registered GPIOs 128 to 143 on device: DaVinci
DaVinci: 144 gpio irqs
print_constraints: dummy:
NET: Registered protocol family 16
EMAC: MII PHY configured
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c-gpio i2c-gpio.1: using pins 20 (SDA) and 21 (SCL)
Advanced Linux Sound Architecture Driver Version 1.0.24.
Switching to clocksource timer0_1
musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
musb-hdrc musb-hdrc: dma type: dma-cppi41
MUSB255 controller's USBSS revision = 4ea11003
Waiting for USB PHY clock good...
musb-hdrc musb-hdrc: USB OTG mode controller at fee00000 using DMA, IRQ 58
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 243
io scheduler noop registered (default)
da8xx_lcdc da8xx_lcdc.0: GLCD: Found VGA_Monitor panel
Console: switching to colour frame buffer device 80x30
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a AR7
serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a AR7
serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a AR7
console [ttyS2] enabled
brd: module loaded
ahci ahci: forcing PORTS_IMPL to 0x1
ahci ahci: AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x01e18000-0x01e19fff] port 0x100 irq 67
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xcc (Micron NAND 512MiB 3,3V 16-bit)
Bad block table found at page 262080, version 0x01
Bad block table found at page 262016, version 0x01
Creating 4 MTD partitions on "davinci_nand.1":
0x000000000000-0x000000020000 : "u-boot env"
0x000000020000-0x0000000a0000 : "u-boot"
0x0000000a0000-0x0000002a0000 : "kernel"
0x0000002a0000-0x000020000000 : "filesystem"
davinci_nand davinci_nand.1: controller rev. 2.5
davinci_mdio davinci_mdio.0: davinci mdio revision 1.5
davinci_mdio davinci_mdio.0: detected phy mask ffffff7f
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[7]: device davinci_mdio-0:07, driver SMSC LAN8710/LAN8720
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
ohci ohci.0: DA8xx OHCI
ohci ohci.0: new USB bus registered, assigned bus number 1
Waiting for USB PHY clock good...
ohci ohci.0: irq 59, io mem 0x01e25000
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
input: gpio-keys-polled as /devices/platform/gpio-keys-polled.0/input/input0
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
omap_rtc: RTC power up reset detected
omap_rtc: already running
i2c /dev entries driver
watchdog watchdog: heartbeat 60 sec
cpuidle: using governor ladder
cpuidle: using governor menu
davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
soc-audio soc-audio.0: ASoC: Failed to create card debugfs directory
_regulator_get: 1-0018 supply IOVDD not found, using dummy regulator
ata1: SATA link down (SStatus 0 SControl 300)
_regulator_get: 1-0018 supply DVDD not found, using dummy regulator
_regulator_get: 1-0018 supply AVDD not found, using dummy regulator
_regulator_get: 1-0018 supply DRVDD not found, using dummy regulator
asoc: tlv320aic3x-hifi <-> davinci-mcasp.0 mapping ok
ALSA device list:
#0: DA850/OMAP-L138 EVM
TCP cubic registered
NET: Registered protocol family 17
console [netcon0] enabled
netconsole: network logging started
davinci_emac davinci_emac.1: using random MAC addr: c2:d8:76:06:6a:bb
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:22:56 UTC (946686176)
Root-NFS: no NFS server address
VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "nfs" or unknown-block(2,0)
Please append a correct "root=" boot option; here are the available partitions:
1f00 128 mtdblock0 (driver?)
1f01 512 mtdblock1 (driver?)
1f02 2048 mtdblock2 (driver?)
1f03 521600 mtdblock3 (driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)