We need to start a ssh server on GC5330 EVM utilizing the OMAP L138. The baseline code we are using is DaVinci-PSP-SDK-03.20.00.12 and we've modified local.conf with the following line (in bold):
# Disable DropBear for now due to export restrictions
DISTRO_SSH_DAEMON = "dropbear"
# Disable all crypt support in curl due to export restrictions
CURL_FEATURES = "zlib,cookies,dict,file,ftp,http,telnet,tftp"
However on a complete rebuild of the kernel (doing correct cleaning), we clearly see that the sshd service NEVER comes up, but clearly the telnetd service comes up. In the task-arago-base.bb we only see - but never see anything with SSH:
ARAGO_BASE = "\
${ARAGO_ALSA_BASE} \
ldd \
mtd-utils \
curl \
arago-feed-configs \
initscript-telnetd \
devmem2 \
"
I'm sure we missed something in some other configuration.