Part Number: AM3358
Other Parts Discussed in Thread: TLV320AIC3111
Tool/software: Linux
Hi,
I've run into an issue with our AM3358 based board, we use a tlv320aic3111 codec for audio which works fine under normal operation however if I suspend the platform (using the supplied pm_suspend.sh) when the device is re-woken the audio no longer plays correctly, the audio is garbled in some way.
We are using the processor SDK v1.03 and do not have an option to move to a newer version, I have checked SDK v3 and the issue does not seem to arise in it. I'm not sure if a bug was spotted at some point here but it would be very helpful if you could point me in the right direction...
Regards
Micheal