Tool/software: Linux
Hi,
The SDK :ti-processor-sdk-linux-am335x-evm-3.02.00.05
HW Platform: TMDSSK3358
I don't want Matrix to run on boot up,so based on the web http://processors.wiki.ti.com/index.php/Matrix_Users_Guide?keyMatch=matrix&tisearch=Search-EN ,from the console I typed the following commands:
cd /etc/rc5.d
mv S97matrix-gui-2.0 K97matrix-gui-2.0
But after reboot,it still started the matrix-gui-2.0 on boot up.
.........
[ OK ] Started telnetd.service.
Starting busybox-udhcpd.service...
Starting thttpd.service...
[ OK ] Started busybox-udhcpd.service.
[ OK ] Started thttpd.service.
Starting rng-tools.service...
[ OK ] Started rng-tools.service.
Starting matrix-gui-2.0.service...
[ OK ] Started matrix-gui-2.0.service.
Starting parse-ip.service...
Starting thermal-zone-init.service...
[ OK ] Started thermal-zone-init.service.
................
So how I can stop the matrix on boot up,thanks.
Best wishes
Jianhua Yuan