Other Parts Discussed in Thread: TUSB2551A, OMAP3525
Hi. We have a custom board which uses an omap3525 and a TUSB2551A transceiver. We have the following set up on the hardware:
omap ------------ transceiver
gpio 100 ------------speed
gpio 101 ------------softcon
gpio 102 -------------suspend
MM1_RXRCV-------RCV
MM1_TXDAT--------VP
MM1_TXSE0--------VM
MM1_TXEN_N-----OE
In U-boot in the mux config what settings do i need for these pins and also what settings do i need to enable in the linux kernel to get this to work (we are using the beagle board kernel currently so I assume we will need to change stuff from that)... Any help would be much appreciated. Please also ask questions if i am being unclear.