This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

x-loader cannot boot from serial



I have a question about x-loader.  Using the beagleboard validation x-loader from http://gitorious.org/beagleboard-validation I can only get it to work if its flashed to NAND. If i serial boot using this there is not input. Once this is flashed to NAND it works fine.  In order to boot serial and get a ukermit prompt for u-boot, i have to use the omap-zoom source for x-loader using a make omap3430labradordownload_config. is there anyway to configure the validation x-loader to work the same way as the omap-zoom source?