Part Number: AM5728
Hi,
There is a question in following eratta of AM5728.
i870 PCIe Unaligned Read Access Issue
2. Set the PCIE_SS1_AXI2OCP_LEGACY_MODE_ENABLE and PCIE_SS2_AXI2OCP_LEGACY_MODE_ENABLE bits to 0x1 in the
CTRL_CORE_SMA_SW_7 Control Module register. This will make all Read TLPs 32- bit aligned with all byte enables set to 1.
When this workaround 2 is used, may the data read as the description of the access of 8bit by the program definitely?
What kind of influence does it have?
Is it transfer throughput and memory size?
Best Regards,
Shigehiro Tsuda