This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM369: DM385

Part Number: TMS320DM369


Hello,

I am having trouble selecting a DaVinci processor for my application. I am deciding between the TMS320DM369 and the DM385. My application is to take Bayer camera input and stream over WiLink 1837 module with some compression (likely MJPEG) in between with 1080p 30 fps max. I believe that both of these processors are capable of this, so I ask:

1. Is one of them more recommended for new designs?

2. Will the lower clock speed of the DM369 likely cause latency issues or is 432 MHz sufficient?

3. Which one does TI recommend?

Thanks.