This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVMK2H: evmK2H, HyperLink, Rack

Part Number: EVMK2H

Hi,

we would like to purchase multiple evmK2H.

Q1: Where can I find out, if it is populated with an ‘06, ‘12 or ‘14 ?

Q2: Is the HyperLink routed through the ACTA connector ?

Q3: Can you recommend a rack to connect multiple evmK2H via HyperLink ?

Q4: Can I use HyperLink and 10bGit at the same time ? What would be the relevant connectors for it on the evmK2H then.

Thank you for your answers in advance.

Regards, TSM