Part Number: TMS320C6657
I am not able to generate an interrupt by setting a bit in an event set register in software (EVTSETn, SPRUGW0C, 9.5.1.2)? Interrupts are working. For example a timer ISR is generated from a hardware driven event 66 (Timer 2 interrupt low) muxed to INT4. However if I don't enable the timer but try to trigger INT4 manually by setting a bit corresponding to event 66 in EVTSET2 it doesn't trigger the interrupt. Is this supposed to work?