This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Starterware/TMS320C6748: How can I change cs1 to cs0 in SPI1 example in c6748 starterware? So far not working.

Part Number: TMS320C6748

Tool/software: Starterware

I changed CS2 to CS0 in C6748 starterware SPI example. However, I don't see any CS0 signal out through oscilloscope. What would be wrong with this code. Any idea? The board is custom made based on C6748 LCDK and CS0 directly connects to DSP.

/**
 * \file spi.c
 *
 * \brief  This is a sample application file which invokes some APIs
 *         from the SPI device abstraction layer to perform configuration,
 *         transmission and reception operations.
 */

/*
* Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/
*
*  Redistribution and use in source and binary forms, with or without
*  modification, are permitted provided that the following conditions
*  are met:
*
*    Redistributions of source code must retain the above copyright
*    notice, this list of conditions and the following disclaimer.
*
*    Redistributions in binary form must reproduce the above copyright
*    notice, this list of conditions and the following disclaimer in the
*    documentation and/or other materials provided with the  
*    distribution.
*
*    Neither the name of Texas Instruments Incorporated nor the names of
*    its contributors may be used to endorse or promote products derived
*    from this software without specific prior written permission.
*
*  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
*  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
*  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
*  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
*  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
*  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
*  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
*  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
*  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
*  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/

#include <string.h>
#include "soc_C6748.h"
#include "hw_psc_C6748.h"
#include "lcdkC6748.h"
#include "uart.h"
#include "spi.h"
#include "psc.h"
#include "interrupt.h"
#include "uartStdio.h"

/******************************************************************************
**                      INTERNAL MACRO DEFINITIONS
*******************************************************************************/
/* value to configure SMIO,SOMI,CLK and CS pin as functional pin */
#define SIMO_SOMI_CLK_CS        0x00000E01
#define CHAR_LENGTH             0x10

/******************************************************************************
**                      INTERNAL FUNCTION PROTOTYPES
*******************************************************************************/
static void SPIConfigDataFmtReg(unsigned int dataFormat);
//static void SpiTransfer(void);
static void SetUpInt(void);
static void SetUpSPI(void);
static void GetStatusCommand(void);
static void ResetCommand(void);
void SPIIsr(void);
void Delay(volatile unsigned int delay);
static void tx_Command(void);

/******************************************************************************
**                      INTERNAL VARIABLE DEFINITIONS
*******************************************************************************/
volatile unsigned int flag = 1;
unsigned int tx_len;
unsigned int rx_len;
unsigned char vrf_data[260];
unsigned char tx_data[260];
volatile unsigned char rx_data[260];
unsigned char *p_tx;
volatile unsigned char *p_rx;
unsigned short *p16_tx;
unsigned short *p16_rx;
unsigned short tx16_data[260];
unsigned short rx16_data[260];

volatile unsigned char StatusResponseMessage[16];

/******************************************************************************
**                      INTERNAL FUNCTION DEFINITIONS
*******************************************************************************/
int main(void)
{
    /* Waking up the SPI1 instance. */
    PSCModuleControl(SOC_PSC_0_REGS, HW_PSC_SPI0, PSC_POWERDOMAIN_ALWAYS_ON,
                     PSC_MDCTL_NEXT_ENABLE);

    /* Initializing the UART instance for serial communication. */
    UARTStdioInit();

    UARTPuts("Welcome to StarterWare SPI application.\r\n\r\n", -1);
    UARTPuts("Here the SPI controller on the SoC communicates with", -1);
    UARTPuts(" the Fingerprint Sensor present on the LCDK.\r\n\r\n", -1);

    /* Performing the Pin Multiplexing for SPI1. */
    SPIPinMuxSetup(1);

    /*
    ** Using the Chip Select(CS) 0 pin of SPI1 to communicate with the Fingerprint Sensor.
    */
    SPI1CSPinMuxSetup(0); // Select CS0

    /* Enable use of SPI1 interrupts. */
    SetUpInt();

    /* Configuring and enabling the SPI1 instance. */
    SetUpSPI();

    /* Issue a Reset to the Fingerprint Sensor */
//    ResetCommand();

    tx_Command();

//  UARTPuts("Attempting to Reset the Fingerprint Sensor.\r\n\r\n", -1);
    SPITransmitData1(SOC_SPI_0_REGS,tx16_data[0]);
    printf("Sent data[0] is %x\n",tx16_data[0]);
//    Delay(10000000);
    SPITransmitData1(SOC_SPI_0_REGS,tx16_data[1]);
    printf("Sent data[1] is %x\n",tx16_data[1]);
//    Delay(10000000);
    SPITransmitData1(SOC_SPI_0_REGS,tx16_data[0]);
    printf("Sent data[0] is %x\n",tx16_data[0]);
//    Delay(10000000);
    SPITransmitData1(SOC_SPI_0_REGS,tx16_data[2]);
    printf("Sent data[2] is %x\n",tx16_data[2]);
//    Delay(10000000);
    while(1)
    {
        SPITransmitData1(SOC_SPI_0_REGS,tx16_data[0]);
        printf("Sent data[0] is %x\n",tx16_data[0]);
//        Delay(10000000);
        SPITransmitData1(SOC_SPI_0_REGS,tx16_data[3]);
        printf("Sent data[3] is %x\n",tx16_data[3]);
//        Delay(10000000);
    }

    /* Read the Status of the Fingerprint Sensor */
    /*
    GetStatusCommand();
    if(StatusResponseMessage[11] == 0x48)
    {
        UARTPuts("Fingerprint Sensor Successfully Reset.\r\n\r\n", -1);
    }
    else
    {
        UARTPuts("ERROR: Fingerprint Sensor Reset Attempt Unsuccessful.\r\n\r\n", -1);
    }
    */
}

static void tx_Command(void)
{
 // Command list
 tx16_data[0] = 0x8001; // Select REG01
 tx16_data[1] = 0x0001; // Set Software Reset
 tx16_data[2] = 0x0000; // reset software Reset
 tx16_data[3] = 0x0080; // Set display on
}

static void GetStatusCommand(void)
{
 unsigned int i;

 // Issue Get Status command and read Status Message Response
 tx_data[0] = 0x80;
 tx_data[1] = 0x10;
 tx_data[2] = 0xBA;
 tx_data[3] = 0x07;
 tx_data[4] = 0x00;
 tx_data[5] = 0x00;
 tx_data[6] = 0x00;
 tx_data[7] = 0xFF;
 tx_data[8] = 0xFF;
 tx_data[9] = 0xFF;
 tx_data[10] = 0xFF;
 tx_data[11] = 0xFF;
 tx_data[12] = 0xFF;
 tx_data[13] = 0xFF;
 tx_data[14] = 0xFF;
 tx_data[15] = 0xFF;
 tx_data[16] = 0xFF;
 tx_data[17] = 0xFF;
 tx_data[18] = 0xFF;
 tx_data[19] = 0xFF;
 tx_data[20] = 0xFF;
 tx_data[21] = 0xFF;
 tx_data[22] = 0xFF;
 tx_len = 23;
 rx_len = 23;

 SPIDat1Config(SOC_SPI_0_REGS, (SPI_CSHOLD | SPI_DATA_FORMAT0), 0x1);
    SpiTransfer();

    for(i=0;i<16;i++)
    {
     StatusResponseMessage[i] = rx_data[i+7];
    }
}

static void ResetCommand(void)
{
 // Issue Reset Command
 tx_data[0] = 0x80;
 tx_data[1] = 0x14;
 tx_data[2] = 0xBA;
 tx_data[3] = 0x07;
 tx_data[4] = 0x00;
 tx_data[5] = 0x00;
 tx_data[6] = 0x00;

 tx_len = 7;
 rx_len = 7;

 SPIDat1Config(SOC_SPI_0_REGS, (SPI_CSHOLD | SPI_DATA_FORMAT0), 0x1);
    SpiTransfer();
}

/*
** Configures ARM interrupt controller to generate SPI interrupt
**
*/
static void SetUpInt(void)
{
 // Setup the ARM or DSP interrupt controller

#ifdef _TMS320C6X
 // Initialize the DSP interrupt controller
 IntDSPINTCInit();

 // Register the ISR in the vector table
 IntRegister(C674X_MASK_INT4, SPIIsr);

 // Map system interrupt to the DSP maskable interrupt
 IntEventMap(C674X_MASK_INT4, SYS_INT_SPI1_INT);

 // Enable the DSP maskable interrupt
 IntEnable(C674X_MASK_INT4);

 // Enable DSP interrupts globally
 IntGlobalEnable();
#else
    /* Initialize the ARM Interrupt Controller.*/
    IntAINTCInit();

    /* Register the ISR in the Interrupt Vector Table.*/
    IntRegister(SYS_INT_SPINT1, SPIIsr);

    /* Set the channnel number 2 of AINTC for system interrupt 56.
     * Channel 2 is mapped to IRQ interrupt of ARM9.
    */
    IntChannelSet(SYS_INT_SPINT1, 2);

    /* Enable the System Interrupts for AINTC.*/
    IntSystemEnable(SYS_INT_SPINT1);

    /* Enable IRQ in CPSR.*/
    IntMasterIRQEnable();

    /* Enable the interrupts in GER of AINTC.*/
    IntGlobalEnable();

    /* Enable the interrupts in HIER of AINTC.*/
    IntIRQEnable();
#endif
}

/*
** Configures SPI Controller
**
*/
static void SetUpSPI(void)
{
    unsigned char cs  = 0x01;
    unsigned char dcs = 0x01;
    unsigned int  val = SIMO_SOMI_CLK_CS;
    SPIReset(SOC_SPI_0_REGS);

    SPIOutOfReset(SOC_SPI_0_REGS);

    SPIModeConfigure(SOC_SPI_0_REGS, SPI_MASTER_MODE);

    //SPIClkConfigure(SOC_SPI_0_REGS, 150000000, 20000000, SPI_DATA_FORMAT0);
    SPIClkConfigure(SOC_SPI_0_REGS, 150000000, 1000000, SPI_DATA_FORMAT0);

    SPIPinControl(SOC_SPI_0_REGS, 0, 0, &val);

    SPIDefaultCSSet(SOC_SPI_0_REGS, dcs);

    /* Configures SPI Data Format Register */
    SPIConfigDataFmtReg(SPI_DATA_FORMAT0);
 
     /* Selects the SPI Data format register to used and Sets CSHOLD
      * to assert CS pin(line) 
      */
    SPIDat1Config(SOC_SPI_0_REGS, (SPI_CSHOLD | SPI_DATA_FORMAT0), cs);

     /* map interrupts to interrupt line INT1 */
    SPIIntLevelSet(SOC_SPI_0_REGS, SPI_RECV_INTLVL | SPI_TRANSMIT_INTLVL);
   
    /* Enable SPI communication */
    SPIEnable(SOC_SPI_0_REGS);
}
/*
** Configures Data Format register of SPI
**
*/
static void SPIConfigDataFmtReg(unsigned int dataFormat)
{
    /* Configures the polarity and phase of SPI clock */

 SPIConfigClkFormat(SOC_SPI_0_REGS,
                       (SPI_CLK_POL_HIGH | SPI_CLK_INPHASE),
                       dataFormat);

 /*
    SPIConfigClkFormat(SOC_SPI_0_REGS,
                       (SPI_CLK_POL_LOW | SPI_CLK_INPHASE),
                       dataFormat);
    */

    /* Configures SPI to transmit MSB bit First during data transfer */
    SPIShiftMsbFirst(SOC_SPI_0_REGS, dataFormat);

    /* Sets the Charcter length */
    SPICharLengthSet(SOC_SPI_0_REGS, CHAR_LENGTH, dataFormat);
}

/*
** Enables SPI Transmit and Receive interrupt.
** Deasserts Chip Select line.
*/


static void  SpiTransfer(void)
{
    p_tx = &tx_data[0];
    p_rx = &rx_data[0];
    SPIIntEnable(SOC_SPI_0_REGS, (SPI_RECV_INT | SPI_TRANSMIT_INT));
    while(flag);
    flag = 1;
    /* Deasserts the CS pin(line) */
    SPIDat1Config(SOC_SPI_0_REGS, SPI_DATA_FORMAT0, 0x1);
}

/*
** Data transmission and receiption SPIIsr
**
*/
void SPIIsr(void)
{
    unsigned int intCode = 0;

#ifdef _TMS320C6X
    IntEventClear(SYS_INT_SPI1_INT);
#else
    IntSystemStatusClear(56);
#endif

    intCode = SPIInterruptVectorGet(SOC_SPI_0_REGS);

    while (intCode)
    {
        if(intCode == SPI_TX_BUF_EMPTY)
        {
            tx_len--;
            SPITransmitData1(SOC_SPI_0_REGS, *p_tx);
            p_tx++;
            if (!tx_len)
            {
                SPIIntDisable(SOC_SPI_0_REGS, SPI_TRANSMIT_INT);
            }
        }

        if(intCode == SPI_RECV_FULL)
        {
            rx_len--;
            *p_rx = (char)SPIDataReceive(SOC_SPI_0_REGS);
            p_rx++;
            if (!rx_len)
            {
                flag = 0;
                SPIIntDisable(SOC_SPI_0_REGS, SPI_RECV_INT);
            }
        }

        intCode = SPIInterruptVectorGet(SOC_SPI_0_REGS);
    }
}

/* Delay Function */

void Delay(volatile unsigned int delay)
{
    while(delay--);
}


/******************************* End of file *********************************/

  • Your thread title implies you are tryring to use SPI1. You have a mix of SPI0 and SPI1 references. Example, this line

    PSCModuleControl(SOC_PSC_0_REGS, HW_PSC_SPI0, PSC_POWERDOMAIN_ALWAYS_ON,
    PSC_MDCTL_NEXT_ENABLE);
    should be:

    PSCModuleControl(SOC_PSC_1_REGS, HW_PSC_SPI1, PSC_POWERDOMAIN_ALWAYS_ON,
    PSC_MDCTL_NEXT_ENABLE);

    For now, it should not matter as the GEL script probably powers and clocks all peripherals.

    Lines like
    SPITransmitData1(SOC_SPI_0_REGS,tx16_data[0]);
    should have SOC_SPI_1_REGS instead. I don't think you call SPITransmitData1 directly like that. There are a lot of SOC_SPI_0_REGS references that should be SOC_SPI_1_REGS.
  • It is working. Thank you, Norman.