Part Number: AM3358
Other Parts Discussed in Thread: AMIC110
Tool/software: Linux
I am attempting to do USB HS signal quality testing on AM3358 as host. (BBB clone that can run various versions of Linux.)
1. I see in the AM335x and AMIC110 Sitara Processors TRM (SPRUH73O) section 16.3.10 that one can enter test mode and output high-speed test packet for signal quality testing. However there appears to be no mention of a TESTMODE register in the TRM. Is there a test mode register, or is this not implemented in AM3358?
2. If supported and there is not a Linux driver readily available, is it possible to manually send commands as shown “IN Host Mode” in the following link?
http://processors.wiki.ti.com/index.php/USB_Test_Mode_on_DWC3
What would those registers be?
3. Does AM3358 support USB High Speed PID definitions?