This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM368: DM368 UART Booting

Part Number: TMS320DM368

Hi

We are using DM368 on Leopard TB-02. I am trying to boot the DM368 using UART. I didnot find any procedure to boot the board from UART. I have selected the switch settings for the UART. Continouse "BOOT ME" prints are comming in the Console. I am trying to transfer the UBL file using Hyper Terminal. I tried all the transfer modes like X modem, 1K X modem, kermit. File not getting tranferred. I have seen some threads related UART Booting. I have found that others are using some Serial Flashing applications like sfh_DM368.exe and slh_DM36x.exe.


Are these applications are mandatory for the UART Booting ?? If so where can I find these applications for download.

Regards,

Pranay Kumar K