Part Number: AM5718
Tool/software: Linux
Hi TI Experts,
I am a fresh developer for Sitara Processors, I meet one problems for booting the uboot from SD card. I create the SD card by
http://processors.wiki.ti.com/index.php/Processor_SDK_Linux_Creating_a_SD_Card_with_Windows
The image is download from
http://software-dl.ti.com/processor-sdk-linux-rt/esd/AM57X/latest/index_FDS.html
| am57xx-evm-linux-rt-03.02.00.05.img.zip |
According to office doc sprui97.pdf, 4.1 The AM571x IDK EVM is configured by default to 0x8106 to enable UBOOT/Linux boot from the SDCARD.
I using minicom to connect the serial port from the AM571x IDK EVM, the setting is : baud: 115200 data bits: 8 parity: N Stop Bits: 1.
But I can not seen any log from the minicom terminal. Any problems for my process?
Thanks a lot!
Nemo