Part Number: TMS320C6747
Tool/software: TI-RTOS
TI-RTOS team,
Our customer is working with C6747 on a product that has been in production for some time. They recently changed build environments:
Old:
CCS 3.3
Compiler 7.3.10
DSP/BIOS 5.41
New:
CCS 6.2.0
Compiler 7.4.18
DSP/BIOS 5.42
It looks like there are problems where memory is not initialized as expected when accessing it. They are using MEM_alloc().
They have imported the TCF file from the old project to the new, and are using this to define the heap size. Do you have any advice on moving a project between these build environments?
The problem has already been discussed in another thread here:
e2e.ti.com/.../582283
Any other advice is welcome.
There have been some changes to the code as well, so we can't rule that out.
Thanks,
Darren