Part Number: DRA744
Other Parts Discussed in Thread: CDCM9102
My customer is developing a cluster using our JAC DRA744 and they need to connect the DRA744 with a WiFi module
the Wifi module is operating with LVPECL ; the Jac DRA744 port is an HCSL , in order to manage the two different specification (modem LVPECL and DRA744 HCSL) I have proposed CDCM9102 But , question is : do we need to add a buffer form Jac DRA744 port to the modem? Or the fan out of Jac DRA744 is able to manage the interface w/o any external buffer ? The connection lenght is 200mm
, but I need your help to figure out if we have to add an external buffer
I need also another information on top of the here below request.
> Is the 100Mhz clock available for external clock driver ?
> I am asking since I am going to decide what is the best solution for the external clock driver
>