This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C5505: Not able to move ahead Erase Chip.. (NOR)

Part Number: TMS320C5505

Tool/software: Code Composer Studio

I have created .bin file from. out file using hex conversion utility (hex55.exe).

I am using the DOS command:

hex55 -i filename.out -o boot_image_file_name.bin -boot -v5505 -b -serial8

However, I am unable to upload the boot image (*.bin) into into the NOR Flash.


The programmer I am using is the programmer_c5515_eZdsp.out.


Attached is the screen shot my screen.

The program stuck at the ERASING CHIP..(NOR) and doesn't move ahead of it.

Also, there is error that programmer.c is not there.

Kindly suggest me what to do.

Satyajit