This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kernel panic on dvevm6467 board when using NFS

Other Parts Discussed in Thread: PCF8574A, THS7303, THS8200, THS7353, TVP7002

I have a problem setting up the NFS filesystem with the DVEVM6467 eval board.

My Boot arguments are:

bootdelay=3
baudrate=115200
bootfile="uImage"
ipaddr=192.168.191.228
gatewayip=192.168.191.1
netmask=255.255.255.0
serverip=192.168.191.229
bootcmd=nboot 80700000 0 a0000;bootm
hostname=davincitest
nfshost=192.168.191.229
rootpath=/home/smartcam/workdir/filesys
stdin=serial
stdout=serial
stderr=serial
ethaddr=00:0e:99:02:b5:ff
bootargs=console=ttyS0,115200n8 noinitrd rw ip=192.168.191.228:192.168.191.229:192.168.191.1:255.255.255.0:davincitest::off root=/dev/nfs nfsroot=192.168.191.229:/home/smartcam/workdir/filesys,nolock davincihd_capture.channel0_numbuffers=4

So the address of the board is at 192.168.191.228 and the address of the NFS server is 192.168.191.229.

The boot sequence

Starting kernel ...

Uncompressing Linux............................................................................................... done, booting the kernel.
Linux version 2.6.10_mvl401-davinci_evm-PSP_01_30_00_082 (x0096290@linwoodxc22) (gcc version 3.4.3 (MontaVista 3.4.3-25.0.24.0500846 2005-06-04)) #1 Fri Jun 20 20:17:18 IST 2008

CPU: ARM926EJ-Sid(wb) [41069265] revision 5 (ARMv5TEJ)
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Machine: DaVinci DM6467 EVM
Memory policy: ECC disabled, Data cache writeback
DM6467
Built 1 zonelists
Kernel command line: console=ttyS0,115200n8 noinitrd rw ip=192.168.191.228:192.168.191.229:192.168.191.1:255.255.255.0:davincitest::off root=/dev/nfs nfsroot=192.168.191.229:/home/smartcam/workdir/filesys,nolock davincihd_capture.channel0_numbuffers=4
PID hash table entries: 2048 (order: 11, 32768 bytes)
Console: colour dummy device 80x30
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 256MB = 256MB total
Memory: 256384KB available (2379K code, 513K data, 164K init)
Mount-cache hash table entries: 512 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
spawn_desched_task(00000000)
desched cpu_callback 3/00000000
ksoftirqd started up.
desched cpu_callback 2/00000000
desched thread 0 started up.
NET: Registered protocol family 16
DaVinci: 48 gpio irqs
Registering platform device 'serial8250.0'. Parent at platform
Registering platform device 'musb_hdrc'. Parent at platform
DaVinci I2C DEBUG: 20:15:30 Jun 20 2008
Registering platform device 'i2c'. Parent at platform
ch0 default output "COMPOSITE", mode "NTSC"
ch1 default output "", mode ""
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
musb_hdrc: version 2.2a/db-0.4.8 [cppi-dma] [host] [debug=0]
musb_hdrc: ConfigData=0x06 (UTMI-8, dyn FIFOs, SoftConn)
musb_hdrc: MHDRC RTL version 1.500
musb_hdrc: USB Host mode controller at d0800000 using DMA, IRQ 13
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
JFFS2 version 2.2. (NAND) (C) 2001-2003 Red Hat, Inc.
yaffs Jun 20 2008 20:15:06 Installing.
Registering platform device 'DavinciHD_vdce.2'. Parent at platform
CIR device registered successfully               (Major = 253, Minor = 0)<6>Registering platform device 'cir.0'. Parent at platform
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
Registering platform device 'serial8250'. Parent at platform
ttyS0 at MMIO 0x1c20000 (irq = 40) is a ST16654
ttyS1 at MMIO 0x1c20400 (irq = 41) is a ST16650V2
io scheduler noop registered
io scheduler anticipatory registered
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
Registering platform device 'ti_davinci_emac'. Parent at platform
TI DaVinci EMAC: MAC address is 00:0e:99:02:b5:ff
TI DaVinci EMAC Linux version updated 5.0
TI DaVinci EMAC: Installed 1 instances.
netconsole: not configured, aborting
i2c /dev entries driver
Linux video capture interface: v1.00
Registering platform device 'vpif capture.1'. Parent at platform
Registering platform device 'vpif display.1'. Parent at platform
Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2
ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx
MUX: initialized ATAEN
hda: TOSHIBA MK4032GAX, ATA DISK drive
elevator: using anticipatory as default io scheduler
ide0 at 0xe10661f0-0xe10661f7,0xe10663f6 on irq 22
hda: max request size: 1024KiB
hda: 78140160 sectors (40007 MB), CHS=16383/255/63
 hda: hda1 hda2
    ide0: BM-DMA at 0xe1066000-0xe1066007, BIOS settings: hda:pio, hdb:pio
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
mice: PS/2 mouse device common for all mice
Registering Audio Devices. Total communication    peripherals         (ASP) : 2
Codec with ID = 0 on ASP = 0 is initialized.Using minor number :  3
Configuring the McASP as Master
Configuring the McASP 1 for DIT
SPDIF on ASP = 1 isinitialized.Using minor number : 19
NET: Registered protocol family 2
IP: routing cache hash table of 2048 buckets, 16Kbytes
TCP: Hash tables configured (established 16384 bind 32768)
NET: Registered protocol family 1
NET: Registered protocol family 17
IP-Config: Complete:
      device=eth0, addr=192.168.191.228, mask=255.255.255.0, gw=192.168.191.1,
     host=davincitest, domain=, nis-domain=(none),
     bootserver=192.168.191.229, rootserver=192.168.191.229, rootpath=
Looking up port of RPC 100003/2 on 192.168.191.229
Looking up port of RPC 100005/1 on 192.168.191.229
VFS: Mounted root (nfs filesystem).
Freeing init memory: 164K
Warning: unable to open an initial console.
Kernel panic - not syncing: No init found.  Try passing init= option to kernel.

 

On the NFS server the /etc/exports file contains

/home/smartcam/workdir/filesys *(rw,no_root_squash,no_all_squash,sync)

 

The board seems to recognise that there is an NFS server there but seems to ignore the rootpath.

 

Any suggestions?

  • This error has come up many times in the past on the forum, usually the 'Kernel panic - not syncing: No init found.  Try passing init= option to kernel.' means that either your filesystem is corrupted (such as symbolic links broken by using a plain cp to copy it or not being extracted as root) or missing.

    Simon said:
    The board seems to recognise that there is an NFS server there but seems to ignore the rootpath.

    The NFS server itself seems to be working as you suggest, though it is probably taking into account the rootpath or you would be getting some other error, the rootpath= having nothing after it in the kernel boot log is ok.

  • Thanks, I removed the file structure on the host and reinstalled and now the board loads up fine.

    I do have another problem now after compiling and trying to run the demo apps

    I can compile them fine but have trouble when trying to load the CMEM module

    root@davincitest:/# cd opt/dvsdk/dm6467/
    root@davincitest:/opt/dvsdk/dm6467# ./loadmodules.sh
    CMEMK Error: CMEM phys_start (0x87800000) overlaps kernel (0x80000000 -> 0x90000
    000)
    insmod: error inserting 'cmemk.ko': -1 Invalid parameters
    dsplinkk: no version for "struct_module" found: kernel tainted.
    dsplinkk: module license 'DSP/BIOS(TM) LINK' taints kernel.
    DSPLINK Module (1.50) created on Date: Jan  3 2008 Time: 13:16:55
    root@davincitest:/opt/dvsdk/dm6467# lsmod
    Module                  Size  Used by
    dsplinkk               98220  0

    The demo apps won't load due to the CMEM module not being loaded.

    Any help would be most appreciated.

    Cheers,

    Simon

  • http://e2e.ti.com/forums/t/9440.aspx

    Your CMEM driver isn't loading b/c of the reported overlap in memory map.  You need to resolve this memory map issue.

    Chris

  • Hi,

    im user of Davinci DM6467 but i have some problem to boot my EVM: kernel panic, i followed the option recommanded in this forum but the problem is against here. the nfs start well but i think there are a problem below.

    here, the part of getting started guide: Please tell me if im wrong: i followed:

    4) Perform the following commands to create a copy of the target file system with permissions set for writing to the shared area as useracct. Substitute your user name for useracct. If you installed in a location other than /opt/mv_pro_5.0, use your location in the cp command.

    host $ cp -a /opt/mv_pro_5.0/montavista/pro/devkit/arm/v5t_le/target/* .

    here I did: cp -a /opt/mv_pro_5.0/montavista/pro/devkit/arm/v5t_le/target/ /home/thierno/workdir/filesys/ Its correct to copy?

    host $ chown -R useracct opt
    here i did: chown -R thierno /home/thierno/workdir/filesys/ Its correct?

    5) Still as root, edit the /etc/exports file on the host Linux workstation (not the exports file on the target filesystem) using a text editor like gedit, for example:

    host $ gedit /etc/exports 
    no change

    Add the following line for exporting the filesys area, substituting your user name for useracct. Use the full path from root; ~ may not work for exports on all file systems. By editing the exports file you are effectively sharing the folder so that other devices (such as the EVM) can mount it.

    /home/useracct/workdir/filesys *(rw,no_root_squash,no_all_squash,sync)
    no change

    thanks
    Thierno
  • there is a small error in the line: cp
    it is:

    cp -a /opt/mv_pro_5.0/montavista/pro/devkit/arm/v5t_le/target/ /home/thierno/workdir/filesys

    ITs correct for copy ?

    thanks

    thierno

  • thierno,

    the copy looks fine.  However, chown command should be executed on    /home/thierno/workdir/filesys/opt   directory.  I have not tried what would happen if you change ownership of the entire target filesystem (normally has root ownership).  Can you delete filesys directory, recopy the filesystem and only change ownership on this directory? 

    Also, there is still the possibility that your kernel can be corrupt (assuming it is compatible for now); you may want to reflash your kernel (uImage)

  • Juan, thank you again
    but the directory / home / thierno / workdir / filesys / opt does not exist.
    the directory / home / thierno / workdir / filesys  him exist.
    therefore it is chown: chown -R thierno  / home / thierno / workdir / filesys?
    or else: chown-R thierno / home / thierno / opt / mv_pro ...? where the /opt/mv_pro is the installation directory of the target linux software.
    not well detailed in the guide

    Thierno

  • we definitely want the filesys directory and not the other....

    Can you copy your bootlog to a post similar the the person that started this thread?  also a copy of your /etc/exports file may help...

  • hi,

    here  the gedit of my /etc/export file

    /home/thierno/workdir/filesys/ *(rw,no_root_squash,no_all_squash,sync)


    here my printenv

    DM6467 EVM # printenv
    bootdelay=3
    baudrate=115200
    ipaddr=192.168.1.201
    nfshost=192.168.1.164
    rootpath=/home/thierno/workdir/filesys
    bootcmd=nboot 80700000 0 a0000;bootm
    bootargs=mem=120M console=ttyS0,115200n8 root=/dev/nfs rw noinitrd ip=dhcp nfsro
    ot=192.168.1.164:/home/thierno/workdir/filesys,nolock
    stdin=serial
    stdout=serial
    stderr=serial
    ethaddr=00:0e:99:02:b2:68

    Environment size: 348/131068 bytes
    DM6467 EVM # setenv bootcmd '80700000 0 a0000'
    DM6467 EVM # saveenv
    Saving Environment to NAND...
    Erasing Nand...Writing to Nand... done
    DM6467 EVM # boot
    Unknown command '80700000' - try 'help'
    DM6467 EVM # setenv bootcmd 'nboot 80700000 0 a0000;bootm'
    DM6467 EVM # saveenv
    Saving Environment to NAND...
    Erasing Nand...Writing to Nand... done

    here the copy of my bootlog


    DM6467 EVM # boot

    Loading from NAND 128MiB 3,3V 8-bit, offset 0xa0000
       Image Name:   Linux-2.6.10_mvl401-davinci_evm
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    1390892 Bytes =  1.3 MB
       Load Address: 80008000
       Entry Point:  80008000
    ## Booting image at 80700000 ...
       Image Name:   Linux-2.6.10_mvl401-davinci_evm
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    1390892 Bytes =  1.3 MB
       Load Address: 80008000
       Entry Point:  80008000
       Verifying Checksum ... OK
    OK

    Starting kernel ...

    Uncompressing Linux.............................................................
    ................................. done, booting the kernel.
    Linux version 2.6.10_mvl401-davinci_evm (davincihd@psplinux.india.ti.com) (gcc v
    ersion 3.4.3 (MontaVista 3.4.3-25.0.116.0601565 2006-09-20)) #1 Wed Oct 22 19:05
    :32 IST 2008
    CPU: ARM926EJ-Sid(wb) [41069265] revision 5 (ARMv5TEJ)
    CPU0: D VIVT write-back cache
    CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
    CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
    Machine:
    Memory policy: ECC disabled, Data cache writeback
    DM6467
    Built 1 zonelists
    Kernel command line: mem=120M console=ttyS0,115200n8 root=/dev/nfs rw noinitrd i
    p=dhcp nfsroot=192.168.1.164:/home/thierno/workdir/filesys,nolock
    PID hash table entries: 512 (order: 9, 8192 bytes)
    Console: colour dummy device 80x30
    Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
    Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
    Memory: 120MB = 120MB total
    Memory: 118528KB available (2391K code, 505K data, 152K init)
    Mount-cache hash table entries: 512 (order: 0, 4096 bytes)
    CPU: Testing write buffer coherency: ok
    spawn_desched_task(00000000)
    desched cpu_callback 3/00000000
    ksoftirqd started up.
    desched cpu_callback 2/00000000
    desched thread 0 started up.
    NET: Registered protocol family 16
    Registering platform device 'serial8250.0'. Parent at platform
    DaVinci: 48 gpio irqs
    DaVinci I2C DEBUG: 19:03:51 Oct 22 2008
    Registering platform device 'i2c'. Parent at platform
    SCSI subsystem initialized
    usbcore: registered new driver usbfs
    usbcore: registered new driver hub
    musb_hdrc: version 2.2a/db-0.4.8 [cppi-dma] [host] [debug=0]
    Registering platform device 'musb_hdrc'. Parent at platform
    musb_hdrc: USB Host mode controller at c8000000 using DMA, IRQ 13
    musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
    hub 1-0:1.0: USB hub found
    hub 1-0:1.0: 1 port detected
    JFFS2 version 2.2. (NAND) (C) 2001-2003 Red Hat, Inc.
    yaffs Oct 22 2008 19:03:27 Installing.
    Registering platform device 'DavinciHD_vdce.2'. Parent at platform
    Consumer IR INFO: CIR device registered successfully (Major = 253, Minor = 0)
    Registering platform device 'cir.0'. Parent at platform
    Consumer IR INFO: CIR IRQ 42 registered successfully
    Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
    Registering platform device 'serial8250'. Parent at platform
    ttyS0 at MMIO 0x1c20000 (irq = 40) is a ST16654
    ttyS1 at MMIO 0x1c20400 (irq = 41) is a ST16650V2
    io scheduler noop registered
    io scheduler anticipatory registered
    RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
    Registering platform device 'ti_davinci_emac'. Parent at platform
    TI DaVinci EMAC: MAC address is 00:0e:99:02:b2:68
    TI DaVinci EMAC Linux version updated 5.0
    TI DaVinci EMAC: Installed 1 instances.
    netconsole: not configured, aborting
    i2c /dev entries driver
    Linux video capture interface: v1.00
    Registering platform device 'vpif capture.1'. Parent at platform
    Registering platform device 'vpif display.1'. Parent at platform
    Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2
    ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx
    MUX: initialized ATAEN
    hda: TOSHIBA MK4032GAX, ATA DISK drive
    elevator: using anticipatory as default io scheduler
    ide0 at 0xe10661f0-0xe10661f7,0xe10663f6 on irq 22
    hda: max request size: 1024KiB
    hda: 78140160 sectors (40007 MB), CHS=16383/255/63
     hda: hda1 hda2
        ide0: BM-DMA at 0xe1066000-0xe1066007, BIOS settings: hda:pio, hdb:pio
    Initializing USB Mass Storage driver...
    usbcore: registered new driver usb-storage
    USB Mass Storage support registered.
    mice: PS/2 mouse device common for all mice
    Registering Audio Devices. Total communication peripherals (ASP) : 2
    Codec with ID = 0 on ASP = 0 is initialized.Using minor number :  3
    Configuring the McASP as Master
    Configuring the McASP 1 for DIT
    SPDIF on ASP = 1 is initialized.Using minor number : 19
    NET: Registered protocol family 2
    IP: routing cache hash table of 512 buckets, 4Kbytes
    TCP: Hash tables configured (established 8192 bind 16384)
    NET: Registered protocol family 1
    NET: Registered protocol family 17
    Sending DHCP requests ..., OK
    IP-Config: Got DHCP answer from 0.0.0.0, my address is 192.168.1.170
    IP-Config: Complete:
          device=eth0, addr=192.168.1.170, mask=255.255.255.0, gw=192.168.1.254,
         host=192.168.1.170, domain=, nis-domain=(none),
         bootserver=0.0.0.0, rootserver=192.168.1.164, rootpath=
    Looking up port of RPC 100003/2 on 192.168.1.164
    Looking up port of RPC 100005/1 on 192.168.1.164
    VFS: Mounted root (nfs filesystem).
    Freeing init memory: 152K
    Warning: unable to open an initial console.
    Kernel panic - not syncing: No init found.  Try passing init= option to kernel

     

    thierno

  • According to  your boot-log, your kernel appears to be an older MV pro 4 (based on 2.6.10 kernel)

    bah thierno said:


    Uncompressing Linux.............................................................
    ................................. done, booting the kernel.
    Linux version 2.6.10_mvl401-davinci_evm

    However, your copy command above suggests your file system is based on MV Pro 5 kernel... This could certainly explain the issue.  Both kernel and file-system must come from same DVSDK release.  Please upgrade your kernel to MV Pro 5 and this should help resolve the issue.

  • hi,
    I still have not received my score card DM6467T, I always use the DM6467 card (
    This DM has already been used by others).
    I re-installed all soft (mvl5 and dvsdk from ti.com website) but I still have the same problem (kernel panic ...)
    but when I look at the boot log, I see that version remains mvl4.
    how to update the mlv55 in the EVM by serial link from the host linux (where i have all sources). please.
    Thank you in advance
    best regards

  • hello,

    i have a problem to boot my DM6467T with nfs.

    here my printenv

    bootdelay=3
    baudrate=115200
    addclk=setenv bootargs ${bootargs} clkref=${clkref}
    ethaddr=00:0e:99:02:b6:c0
    ethact=DaVinci EMAC
    clkref=33000000
    nfshost=192.168.1.155
    rootpath=/home/thierno/workdir/filesys
    gateway=192.168.1.255
    filesize=1F7408
    fileaddr=80700000
    gatewayip=192.168.1.254
    netmask=255.255.255.0
    ipaddr=192.168.1.165
    dnsip=192.168.1.254
    serverip=192.168.1.155
    bootfile=uImage-dm6467t-evm.bin
    bootcmd=nboot 0x80700000 0 0x160000;bootm
    bootargs=mem=112M

    console=ttyS0,115200n8 root=/dev/nfs nfsroot=$(nfshost):$(root
    path),nolock ip=dhcp vpif_display.ch2_numbuffers=0 vpif_display.ch3_numbuffers=0

    stdin=serial
    stdout=serial
    stderr=serial
    ver=U-Boot 2009.08 (Jan 20 2010 - 15:19:56)

    Environment size: 689/16380 bytes

    here my bootlog

    Booting PSP Boot Loader

    Starting NAND Copy

    Booting Application @ 0x81080000


    U-Boot 2009.08 (Jan 20 2010 - 15:19:56)

    I2C:   ready
    DRAM:  256 MB
    NAND:  128 MiB
    In:    serial
    Out:   serial
    Err:   serial
    ARM Clock :- 495MHz
    DDR Clock :- 396MHz
    Net:   Ethernet PHY: GENERIC @ 0x01
    DaVinci EMAC
    Hit any key to stop autoboot:  0

    Loading from NAND 128MiB 3,3V 8-bit, offset 0x160000
       Image Name:   Arago/2.6.31+2.6.32-rc1-r31+gitr
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    2061256 Bytes =  2 MB
       Load Address: 80008000
       Entry Point:  80008000
    ## Booting kernel from Legacy Image at 80700000 ...
       Image Name:   Arago/2.6.31+2.6.32-rc1-r31+gitr
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    2061256 Bytes =  2 MB
       Load Address: 80008000
       Entry Point:  80008000
       Verifying Checksum ... OK
       Loading Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux.........................................................
    Booting PSP Boot Loader

    Starting NAND Copy

    Booting Application @ 0x81080000


    U-Boot 2009.08 (Jan 20 2010 - 15:19:56)

    I2C:   ready
    DRAM:  256 MB
    NAND:  128 MiB
    In:    serial
    Out:   serial
    Err:   serial
    ARM Clock :- 495MHz
    DDR Clock :- 396MHz
    Net:   Ethernet PHY: GENERIC @ 0x01
    DaVinci EMAC
    Hit any key to stop autoboot:  0
    DM6467 EVM >
    Booting PSP Boot Loader

    Starting NAND Copy

    Booting Application @ 0x81080000


    U-Boot 2009.08 (Jan 20 2010 - 15:19:56)

    I2C:   ready
    DRAM:  256 MB
    NAND:  128 MiB
    In:    serial
    Out:   serial
    Err:   serial
    ARM Clock :- 495MHz
    DDR Clock :- 396MHz
    Net:   Ethernet PHY: GENERIC @ 0x01
    DaVinci EMAC
    Hit any key to stop autoboot:  0

    Loading from NAND 128MiB 3,3V 8-bit, offset 0x160000
       Image Name:   Arago/2.6.31+2.6.32-rc1-r31+gitr
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    2061256 Bytes =  2 MB
       Load Address: 80008000
       Entry Point:  80008000
    ## Booting kernel from Legacy Image at 80700000 ...
       Image Name:   Arago/2.6.31+2.6.32-rc1-r31+gitr
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    2061256 Bytes =  2 MB
       Load Address: 80008000
       Entry Point:  80008000
       Verifying Checksum ... OK
       Loading Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux.............................................................
    ......................................................................... done,
    booting the kernel.
    Linux version 2.6.32-rc2-davinci1 (denis@elrond) (gcc version 4.3.3 (Sourcery G+
    + Lite 2009q1-203) ) #1 PREEMPT Mon Jan 11 21:45:54 EST 2010
    CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
    CPU: VIVT data cache, VIVT instruction cache
    Machine: DaVinci DM646x EVM
    Memory policy: ECC disabled, Data cache writeback
    DaVinci dm6467_rev3.x variant 0x1
    Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 28448
    Kernel command line: mem=112M console=ttyS0,115200n8 root=/dev/nfs nfsroot=$(nfs
    host):$(rootpath),nolock ip=dhcp vpif_display.ch2_numbuffers=0 vpif_display.ch3_
    numbuffers=0
    PID hash table entries: 512 (order: -1, 2048 bytes)
    Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
    Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
    Memory: 112MB = 112MB total
    Memory: 109140KB available (3876K code, 335K data, 144K init, 0K highmem)
    SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    Hierarchical RCU implementation.
    NR_IRQS:245
    Console: colour dummy device 80x30
    Calibrating delay loop... 246.57 BogoMIPS (lpj=1232896)
    Mount-cache hash table entries: 512
    CPU: Testing write buffer coherency: ok
    DaVinci: 43 gpio irqs
    NET: Registered protocol family 16
    MUX: Setting register STSOMUX_DISABLE
               PINMUX0 (0x00000000) = 0x00000000 -> 0x00000000
    MUX: Setting register STSIMUX_DISABLE
               PINMUX0 (0x00000000) = 0x00000000 -> 0x00000000
    MUX: Setting register PTSOMUX_DISABLE
               PINMUX0 (0x00000000) = 0x00000000 -> 0x00000000
    MUX: Setting register PTSIMUX_DISABLE
               PINMUX0 (0x00000000) = 0x00000000 -> 0x00000000
    MUX: initialized CIR_UART2
    MUX: Setting register CIR_UART2
               PINMUX1 (0x00000004) = 0x00000000 -> 0x00000020
    MUX: initialized ATAEN
    MUX: Setting register ATAEN
               PINMUX0 (0x00000000) = 0x00000000 -> 0x00000001
    bio: create slab <bio-0> at 0
    SCSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    pcf857x 1-0038: gpios 145..152 on a pcf8574a
    pcf857x 1-0038: setup --> -38
    vpif vpif: vpif probe success
    Switching to clocksource timer0_1
    musb_hdrc: version 6.0, pio, peripheral, debug=0
    musb_hdrc: USB Peripheral mode controller at fec64000 using PIO, IRQ 13
    NET: Registered protocol family 2
    IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
    TCP established hash table entries: 4096 (order: 3, 32768 bytes)
    TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
    TCP: Hash tables configured (established 4096 bind 4096)
    TCP reno registered
    NET: Registered protocol family 1
    RPC: Registered udp transport module.
    RPC: Registered tcp transport module.
    RPC: Registered tcp NFSv4.1 backchannel transport module.
    JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
    msgmni has been set to 213
    io scheduler noop registered
    io scheduler anticipatory registered (default)
    CIR device registered successfully                        (Major = 252,  Minor =
     0)
    Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
    serial8250.0: ttyS0 at MMIO 0x1c20000 (irq = 40) is a ST16654
    console [ttyS0] enabled
    serial8250 serial8250.0: unable to register port at index 1 (IO0 MEM1c20400 IRQ4
    1):
    serial8250 serial8250.0: unable to register port at index 2 (IO0 MEM1c20800 IRQ
    2): -22
    brd: module loaded
    loop: module loaded
    at24 1-0050: 32768 byte 24c256 EEPROM (writable)
    Read MAC addr from EEPROM: 00:0e:99:02:b6:c0
    Uniform Multi-Platform E-IDE driver
    ide-gd driver 1.18
        ide0: MMIO-DMA
    hda: TOSHIBA MK4032GAX, ATA DISK drive
    hda: UDMA/100 mode selected
    ide0 at 0xfec661f0-0xfec661f7,0xfec663f6 on irq 22
    hda: max request size: 512KiB
    hda: 78140160 sectors (40007 MB), CHS=16383/255/63
    hda: cache flushes supported
     hda: hda1 hda2
    NAND device: Manufacturer ID: 0x20, Chip ID: 0xf1 (ST Micro NAND 128MiB 3,3V 8-b
    it)
    Scanning device for bad blocks
    Bad eraseblock 2 at 0x000000040000
    Bad eraseblock 6 at 0x0000000c0000
    Bad eraseblock 9 at 0x000000120000
    Bad eraseblock 11 at 0x000000160000
    Bad eraseblock 13 at 0x0000001a0000
    Bad eraseblock 16 at 0x000000200000
    Bad eraseblock 19 at 0x000000260000
    Bad eraseblock 21 at 0x0000002a0000
    Bad eraseblock 23 at 0x0000002e0000
    Bad eraseblock 25 at 0x000000320000
    Bad eraseblock 27 at 0x000000360000
    Bad eraseblock 29 at 0x0000003a0000
    Bad eraseblock 31 at 0x0000003e0000
    Bad eraseblock 35 at 0x000000460000
    Bad eraseblock 37 at 0x0000004a0000
    Bad eraseblock 39 at 0x0000004e0000
    Bad eraseblock 42 at 0x000000540000
    Bad eraseblock 44 at 0x000000580000
    Bad eraseblock 46 at 0x0000005c0000
    Bad eraseblock 48 at 0x000000600000
    Bad eraseblock 50 at 0x000000640000
    Bad eraseblock 53 at 0x0000006a0000
    Bad eraseblock 56 at 0x000000700000
    Bad eraseblock 59 at 0x000000760000
    Bad eraseblock 61 at 0x0000007a0000
    Bad eraseblock 64 at 0x000000800000
    Bad eraseblock 67 at 0x000000860000
    Bad eraseblock 70 at 0x0000008c0000
    Bad eraseblock 72 at 0x000000900000
    Bad eraseblock 75 at 0x000000960000
    Bad eraseblock 77 at 0x0000009a0000
    Bad eraseblock 80 at 0x000000a00000
    Bad eraseblock 82 at 0x000000a40000
    Bad eraseblock 84 at 0x000000a80000
    Bad eraseblock 87 at 0x000000ae0000
    Bad eraseblock 90 at 0x000000b40000
    Bad eraseblock 92 at 0x000000b80000
    Bad eraseblock 95 at 0x000000be0000
    Bad eraseblock 97 at 0x000000c20000
    Bad eraseblock 100 at 0x000000c80000
    Bad eraseblock 103 at 0x000000ce0000
    Bad eraseblock 105 at 0x000000d20000
    Bad eraseblock 107 at 0x000000d60000
    Bad eraseblock 111 at 0x000000de0000
    Bad eraseblock 114 at 0x000000e40000
    Bad eraseblock 116 at 0x000000e80000
    Bad eraseblock 119 at 0x000000ee0000
    Bad eraseblock 121 at 0x000000f20000
    Bad eraseblock 124 at 0x000000f80000
    Bad eraseblock 126 at 0x000000fc0000
    Bad eraseblock 128 at 0x000001000000
    Bad eraseblock 130 at 0x000001040000
    Bad eraseblock 133 at 0x0000010a0000
    Bad eraseblock 136 at 0x000001100000
    Bad eraseblock 139 at 0x000001160000
    Bad eraseblock 142 at 0x0000011c0000
    Bad eraseblock 144 at 0x000001200000
    Bad eraseblock 146 at 0x000001240000
    Bad eraseblock 148 at 0x000001280000
    Bad eraseblock 150 at 0x0000012c0000
    Bad eraseblock 152 at 0x000001300000
    Bad eraseblock 155 at 0x000001360000
    Bad eraseblock 157 at 0x0000013a0000
    Bad eraseblock 159 at 0x0000013e0000
    Bad eraseblock 161 at 0x000001420000
    Bad eraseblock 163 at 0x000001460000
    Bad eraseblock 166 at 0x0000014c0000
    Bad eraseblock 169 at 0x000001520000
    Bad eraseblock 172 at 0x000001580000
    Bad eraseblock 175 at 0x0000015e0000
    Bad eraseblock 177 at 0x000001620000
    Bad eraseblock 179 at 0x000001660000
    Bad eraseblock 182 at 0x0000016c0000
    Bad eraseblock 185 at 0x000001720000
    Bad eraseblock 187 at 0x000001760000
    Bad eraseblock 190 at 0x0000017c0000
    Bad eraseblock 192 at 0x000001800000
    Bad eraseblock 194 at 0x000001840000
    Bad eraseblock 198 at 0x0000018c0000
    Bad eraseblock 200 at 0x000001900000
    Bad eraseblock 202 at 0x000001940000
    Bad eraseblock 205 at 0x0000019a0000
    Bad eraseblock 207 at 0x0000019e0000
    Bad eraseblock 211 at 0x000001a60000
    Bad eraseblock 214 at 0x000001ac0000
    Bad eraseblock 217 at 0x000001b20000
    Bad eraseblock 219 at 0x000001b60000
    Bad eraseblock 222 at 0x000001bc0000
    Bad eraseblock 224 at 0x000001c00000
    Bad eraseblock 226 at 0x000001c40000
    Bad eraseblock 228 at 0x000001c80000
    Bad eraseblock 230 at 0x000001cc0000
    Bad eraseblock 233 at 0x000001d20000
    Bad eraseblock 235 at 0x000001d60000
    Bad eraseblock 238 at 0x000001dc0000
    Bad eraseblock 241 at 0x000001e20000
    Bad eraseblock 244 at 0x000001e80000
    Bad eraseblock 247 at 0x000001ee0000
    Bad eraseblock 249 at 0x000001f20000
    Bad eraseblock 251 at 0x000001f60000
    Bad eraseblock 254 at 0x000001fc0000
    Bad eraseblock 259 at 0x000002060000
    Bad eraseblock 262 at 0x0000020c0000
    Bad eraseblock 265 at 0x000002120000
    Bad eraseblock 268 at 0x000002180000
    Bad eraseblock 270 at 0x0000021c0000
    Bad eraseblock 272 at 0x000002200000
    Bad eraseblock 275 at 0x000002260000
    Bad eraseblock 277 at 0x0000022a0000
    Bad eraseblock 280 at 0x000002300000
    Bad eraseblock 282 at 0x000002340000
    Bad eraseblock 285 at 0x0000023a0000
    Bad eraseblock 287 at 0x0000023e0000
    Bad eraseblock 290 at 0x000002440000
    Bad eraseblock 293 at 0x0000024a0000
    Bad eraseblock 296 at 0x000002500000
    Bad eraseblock 298 at 0x000002540000
    Bad eraseblock 300 at 0x000002580000
    Bad eraseblock 303 at 0x0000025e0000
    Bad eraseblock 305 at 0x000002620000
    Bad eraseblock 307 at 0x000002660000
    Bad eraseblock 309 at 0x0000026a0000
    Bad eraseblock 312 at 0x000002700000
    Bad eraseblock 314 at 0x000002740000
    Bad eraseblock 316 at 0x000002780000
    Bad eraseblock 319 at 0x0000027e0000
    Bad eraseblock 321 at 0x000002820000
    Bad eraseblock 324 at 0x000002880000
    Bad eraseblock 327 at 0x0000028e0000
    Bad eraseblock 329 at 0x000002920000
    Bad eraseblock 332 at 0x000002980000
    Bad eraseblock 335 at 0x0000029e0000
    Bad eraseblock 338 at 0x000002a40000
    Bad eraseblock 341 at 0x000002aa0000
    Bad eraseblock 344 at 0x000002b00000
    Bad eraseblock 348 at 0x000002b80000
    Bad eraseblock 350 at 0x000002bc0000
    Bad eraseblock 352 at 0x000002c00000
    Bad eraseblock 354 at 0x000002c40000
    Bad eraseblock 357 at 0x000002ca0000
    Bad eraseblock 359 at 0x000002ce0000
    Bad eraseblock 361 at 0x000002d20000
    Bad eraseblock 365 at 0x000002da0000
    Bad eraseblock 367 at 0x000002de0000
    Bad eraseblock 369 at 0x000002e20000
    Bad eraseblock 371 at 0x000002e60000
    Bad eraseblock 373 at 0x000002ea0000
    Bad eraseblock 375 at 0x000002ee0000
    Bad eraseblock 378 at 0x000002f40000
    Bad eraseblock 381 at 0x000002fa0000
    Bad eraseblock 384 at 0x000003000000
    Bad eraseblock 387 at 0x000003060000
    Bad eraseblock 389 at 0x0000030a0000
    Bad eraseblock 393 at 0x000003120000
    Bad eraseblock 397 at 0x0000031a0000
    Bad eraseblock 399 at 0x0000031e0000
    Bad eraseblock 402 at 0x000003240000
    Bad eraseblock 405 at 0x0000032a0000
    Bad eraseblock 407 at 0x0000032e0000
    Bad eraseblock 409 at 0x000003320000
    Bad eraseblock 411 at 0x000003360000
    Bad eraseblock 414 at 0x0000033c0000
    Bad eraseblock 416 at 0x000003400000
    Bad eraseblock 419 at 0x000003460000
    Bad eraseblock 422 at 0x0000034c0000
    Bad eraseblock 424 at 0x000003500000
    Bad eraseblock 428 at 0x000003580000
    Bad eraseblock 432 at 0x000003600000
    Bad eraseblock 434 at 0x000003640000
    Bad eraseblock 436 at 0x000003680000
    Bad eraseblock 438 at 0x0000036c0000
    Bad eraseblock 441 at 0x000003720000
    Bad eraseblock 443 at 0x000003760000
    Bad eraseblock 445 at 0x0000037a0000
    Bad eraseblock 448 at 0x000003800000
    Bad eraseblock 451 at 0x000003860000
    Bad eraseblock 455 at 0x0000038e0000
    Bad eraseblock 457 at 0x000003920000
    Bad eraseblock 459 at 0x000003960000
    Bad eraseblock 461 at 0x0000039a0000
    Bad eraseblock 463 at 0x0000039e0000
    Bad eraseblock 465 at 0x000003a20000
    Bad eraseblock 468 at 0x000003a80000
    Bad eraseblock 472 at 0x000003b00000
    Bad eraseblock 474 at 0x000003b40000
    Bad eraseblock 477 at 0x000003ba0000
    Bad eraseblock 479 at 0x000003be0000
    Bad eraseblock 482 at 0x000003c40000
    Bad eraseblock 484 at 0x000003c80000
    Bad eraseblock 486 at 0x000003cc0000
    Bad eraseblock 489 at 0x000003d20000
    Bad eraseblock 492 at 0x000003d80000
    Bad eraseblock 494 at 0x000003dc0000
    Bad eraseblock 497 at 0x000003e20000
    Bad eraseblock 499 at 0x000003e60000
    Bad eraseblock 502 at 0x000003ec0000
    Bad eraseblock 505 at 0x000003f20000
    Bad eraseblock 508 at 0x000003f80000
    Bad eraseblock 510 at 0x000003fc0000
    Bad eraseblock 512 at 0x000004000000
    Bad eraseblock 514 at 0x000004040000
    Bad eraseblock 516 at 0x000004080000
    Bad eraseblock 519 at 0x0000040e0000
    Bad eraseblock 521 at 0x000004120000
    Bad eraseblock 523 at 0x000004160000
    Bad eraseblock 527 at 0x0000041e0000
    Bad eraseblock 529 at 0x000004220000
    Bad eraseblock 531 at 0x000004260000
    Bad eraseblock 533 at 0x0000042a0000
    Bad eraseblock 536 at 0x000004300000
    Bad eraseblock 538 at 0x000004340000
    Bad eraseblock 540 at 0x000004380000
    Bad eraseblock 542 at 0x0000043c0000
    Bad eraseblock 545 at 0x000004420000
    Bad eraseblock 547 at 0x000004460000
    Bad eraseblock 550 at 0x0000044c0000
    Bad eraseblock 553 at 0x000004520000
    Bad eraseblock 556 at 0x000004580000
    Bad eraseblock 558 at 0x0000045c0000
    Bad eraseblock 561 at 0x000004620000
    Bad eraseblock 564 at 0x000004680000
    Bad eraseblock 567 at 0x0000046e0000
    Bad eraseblock 570 at 0x000004740000
    Bad eraseblock 573 at 0x0000047a0000
    Bad eraseblock 575 at 0x0000047e0000
    Bad eraseblock 577 at 0x000004820000
    Bad eraseblock 580 at 0x000004880000
    Bad eraseblock 582 at 0x0000048c0000
    Bad eraseblock 584 at 0x000004900000
    Bad eraseblock 587 at 0x000004960000
    Bad eraseblock 590 at 0x0000049c0000
    Bad eraseblock 592 at 0x000004a00000
    Bad eraseblock 594 at 0x000004a40000
    Bad eraseblock 597 at 0x000004aa0000
    Bad eraseblock 600 at 0x000004b00000
    Bad eraseblock 602 at 0x000004b40000
    Bad eraseblock 605 at 0x000004ba0000
    Bad eraseblock 609 at 0x000004c20000
    Bad eraseblock 611 at 0x000004c60000
    Bad eraseblock 614 at 0x000004cc0000
    Bad eraseblock 616 at 0x000004d00000
    Bad eraseblock 618 at 0x000004d40000
    Bad eraseblock 621 at 0x000004da0000
    Bad eraseblock 623 at 0x000004de0000
    Bad eraseblock 625 at 0x000004e20000
    Bad eraseblock 628 at 0x000004e80000
    Bad eraseblock 630 at 0x000004ec0000
    Bad eraseblock 632 at 0x000004f00000
    Bad eraseblock 634 at 0x000004f40000
    Bad eraseblock 636 at 0x000004f80000
    Bad eraseblock 638 at 0x000004fc0000
    Bad eraseblock 641 at 0x000005020000
    Bad eraseblock 643 at 0x000005060000
    Bad eraseblock 645 at 0x0000050a0000
    Bad eraseblock 648 at 0x000005100000
    Bad eraseblock 650 at 0x000005140000
    Bad eraseblock 652 at 0x000005180000
    Bad eraseblock 655 at 0x0000051e0000
    Bad eraseblock 657 at 0x000005220000
    Bad eraseblock 659 at 0x000005260000
    Bad eraseblock 662 at 0x0000052c0000
    Bad eraseblock 664 at 0x000005300000
    Bad eraseblock 668 at 0x000005380000
    Bad eraseblock 670 at 0x0000053c0000
    Bad eraseblock 672 at 0x000005400000
    Bad eraseblock 674 at 0x000005440000
    Bad eraseblock 677 at 0x0000054a0000
    Bad eraseblock 680 at 0x000005500000
    Bad eraseblock 684 at 0x000005580000
    Bad eraseblock 686 at 0x0000055c0000
    Bad eraseblock 688 at 0x000005600000
    Bad eraseblock 691 at 0x000005660000
    Bad eraseblock 693 at 0x0000056a0000
    Bad eraseblock 695 at 0x0000056e0000
    Bad eraseblock 697 at 0x000005720000
    Bad eraseblock 699 at 0x000005760000
    Bad eraseblock 701 at 0x0000057a0000
    Bad eraseblock 703 at 0x0000057e0000
    Bad eraseblock 706 at 0x000005840000
    Bad eraseblock 708 at 0x000005880000
    Bad eraseblock 711 at 0x0000058e0000
    Bad eraseblock 713 at 0x000005920000
    Bad eraseblock 715 at 0x000005960000
    Bad eraseblock 718 at 0x0000059c0000
    Bad eraseblock 720 at 0x000005a00000
    Bad eraseblock 722 at 0x000005a40000
    Bad eraseblock 725 at 0x000005aa0000
    Bad eraseblock 727 at 0x000005ae0000
    Bad eraseblock 729 at 0x000005b20000
    Bad eraseblock 732 at 0x000005b80000
    Bad eraseblock 735 at 0x000005be0000
    Bad eraseblock 737 at 0x000005c20000
    Bad eraseblock 739 at 0x000005c60000
    Bad eraseblock 741 at 0x000005ca0000
    Bad eraseblock 744 at 0x000005d00000
    Bad eraseblock 746 at 0x000005d40000
    Bad eraseblock 748 at 0x000005d80000
    Bad eraseblock 750 at 0x000005dc0000
    Bad eraseblock 752 at 0x000005e00000
    Bad eraseblock 755 at 0x000005e60000
    Bad eraseblock 757 at 0x000005ea0000
    Bad eraseblock 759 at 0x000005ee0000
    Bad eraseblock 761 at 0x000005f20000
    Bad eraseblock 763 at 0x000005f60000
    Bad eraseblock 766 at 0x000005fc0000
    Bad eraseblock 769 at 0x000006020000
    Bad eraseblock 772 at 0x000006080000
    Bad eraseblock 774 at 0x0000060c0000
    Bad eraseblock 776 at 0x000006100000
    Bad eraseblock 779 at 0x000006160000
    Bad eraseblock 782 at 0x0000061c0000
    Bad eraseblock 785 at 0x000006220000
    Bad eraseblock 788 at 0x000006280000
    Bad eraseblock 790 at 0x0000062c0000
    Bad eraseblock 792 at 0x000006300000
    Bad eraseblock 795 at 0x000006360000
    Bad eraseblock 797 at 0x0000063a0000
    Bad eraseblock 800 at 0x000006400000
    Bad eraseblock 803 at 0x000006460000
    Bad eraseblock 805 at 0x0000064a0000
    Bad eraseblock 808 at 0x000006500000
    Bad eraseblock 811 at 0x000006560000
    Bad eraseblock 813 at 0x0000065a0000
    Bad eraseblock 816 at 0x000006600000
    Bad eraseblock 818 at 0x000006640000
    Bad eraseblock 820 at 0x000006680000
    Bad eraseblock 823 at 0x0000066e0000
    Bad eraseblock 826 at 0x000006740000
    Bad eraseblock 828 at 0x000006780000
    Bad eraseblock 831 at 0x0000067e0000
    Bad eraseblock 834 at 0x000006840000
    Bad eraseblock 837 at 0x0000068a0000
    Bad eraseblock 839 at 0x0000068e0000
    Bad eraseblock 842 at 0x000006940000
    Bad eraseblock 844 at 0x000006980000
    Bad eraseblock 848 at 0x000006a00000
    Bad eraseblock 850 at 0x000006a40000
    Bad eraseblock 853 at 0x000006aa0000
    Bad eraseblock 857 at 0x000006b20000
    Bad eraseblock 859 at 0x000006b60000
    Bad eraseblock 861 at 0x000006ba0000
    Bad eraseblock 864 at 0x000006c00000
    Bad eraseblock 867 at 0x000006c60000
    Bad eraseblock 870 at 0x000006cc0000
    Bad eraseblock 873 at 0x000006d20000
    Bad eraseblock 875 at 0x000006d60000
    Bad eraseblock 878 at 0x000006dc0000
    Bad eraseblock 881 at 0x000006e20000
    Bad eraseblock 883 at 0x000006e60000
    Bad eraseblock 886 at 0x000006ec0000
    Bad eraseblock 888 at 0x000006f00000
    Bad eraseblock 890 at 0x000006f40000
    Bad eraseblock 893 at 0x000006fa0000
    Bad eraseblock 896 at 0x000007000000
    Bad eraseblock 899 at 0x000007060000
    Bad eraseblock 902 at 0x0000070c0000
    Bad eraseblock 905 at 0x000007120000
    Bad eraseblock 907 at 0x000007160000
    Bad eraseblock 909 at 0x0000071a0000
    Bad eraseblock 911 at 0x0000071e0000
    Bad eraseblock 913 at 0x000007220000
    Bad eraseblock 916 at 0x000007280000
    Bad eraseblock 918 at 0x0000072c0000
    Bad eraseblock 921 at 0x000007320000
    Bad eraseblock 924 at 0x000007380000
    Bad eraseblock 929 at 0x000007420000
    Bad eraseblock 932 at 0x000007480000
    Bad eraseblock 934 at 0x0000074c0000
    Bad eraseblock 936 at 0x000007500000
    Bad eraseblock 939 at 0x000007560000
    Bad eraseblock 942 at 0x0000075c0000
    Bad eraseblock 944 at 0x000007600000
    Bad eraseblock 947 at 0x000007660000
    Bad eraseblock 950 at 0x0000076c0000
    Bad eraseblock 952 at 0x000007700000
    Bad eraseblock 956 at 0x000007780000
    Bad eraseblock 959 at 0x0000077e0000
    Bad eraseblock 961 at 0x000007820000
    Bad eraseblock 964 at 0x000007880000
    Bad eraseblock 967 at 0x0000078e0000
    Bad eraseblock 969 at 0x000007920000
    Bad eraseblock 973 at 0x0000079a0000
    Bad eraseblock 975 at 0x0000079e0000
    Bad eraseblock 977 at 0x000007a20000
    Bad eraseblock 980 at 0x000007a80000
    Bad eraseblock 982 at 0x000007ac0000
    Bad eraseblock 985 at 0x000007b20000
    Bad eraseblock 987 at 0x000007b60000
    Bad eraseblock 989 at 0x000007ba0000
    Bad eraseblock 993 at 0x000007c20000
    Bad eraseblock 995 at 0x000007c60000
    Bad eraseblock 999 at 0x000007ce0000
    Bad eraseblock 1003 at 0x000007d60000
    Bad eraseblock 1005 at 0x000007da0000
    Bad eraseblock 1007 at 0x000007de0000
    Bad eraseblock 1010 at 0x000007e40000
    Bad eraseblock 1012 at 0x000007e80000
    Bad eraseblock 1014 at 0x000007ec0000
    Bad eraseblock 1016 at 0x000007f00000
    Bad eraseblock 1019 at 0x000007f60000
    Bad eraseblock 1021 at 0x000007fa0000
    Creating 4 MTD partitions on "davinci_nand.0":
    0x000000000000-0x000000020000 : "params"
    0x000000020000-0x000000160000 : "bootloader"
    0x000000160000-0x000000560000 : "kernel"
    0x000000560000-0x000008000000 : "filesystem"
    davinci_nand davinci_nand.0: controller rev. 2.2
    spi_davinci spi_davinci.0: DaVinci SPI driver in EDMA mode
    Using RX channel = 17 , TX channel = 16 and event queue = 3
    at25 spi0.0: 32 KByte at25640a eeprom, pagesize 64
    spi_davinci spi_davinci.0: Controller at 0xfec66800
    PPP generic driver version 2.4.2
    PPP Deflate Compression module registered
    tun: Universal TUN/TAP device driver, 1.6
    tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
    dm9000 Ethernet Driver, V1.31
    console [netcon0] enabled
    netconsole: network logging started
    Initializing USB Mass Storage driver...
    usbcore: registered new interface driver usb-storage
    USB Mass Storage support registered.
    usbcore: registered new interface driver usbtest
    g_ether gadget: using random self ethernet address
    g_ether gadget: using random host ethernet address
    usb0: MAC 02:45:76:90:c8:65
    usb0: HOST MAC c2:84:9d:58:12:c1
    g_ether gadget: Ethernet Gadget, version: Memorial Day 2008
    g_ether gadget: g_ether ready
    i2c /dev entries driver
    Linux video capture interface: v2.00
    ths7303 1-002c: chip found @ 0x58 (DaVinci I2C adapter)
    ths8200 1-0020: chip found @ 0x40 (DaVinci I2C adapter)
    ths7353 1-002e: chip found @ 0x5c (DaVinci I2C adapter)
    vpif_capture vpif_capture: registered sub device ths7353
    tvp7002 1-005d: tvp7002 1-005d decoder driver registered !!
    vpif_capture vpif_capture: registered sub device tvp7002
    vpif_capture vpif_capture: DM646x VPIF Capture driver initialized
    watchdog watchdog: heartbeat 60 sec
    usbcore: registered new interface driver usbhid
    usbhid: v2.6:USB HID core driver
    Advanced Linux Sound Architecture Driver Version 1.0.21.
    No device for DAI tlv320aic3x
    asoc: tlv320aic3x <-> davinci-i2s mapping ok
    asoc: DIT <-> davinci-dit mapping ok
    ALSA device list:
      #0: DaVinci DM6467 EVM (tlv320aic3x)
    TCP cubic registered
    NET: Registered protocol family 17
    Clocks: disable unused uart1
    Clocks: disable unused emac
    Clocks: disable unused timer1
    emac-mii: probed
    drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
    eth0: attached PHY driver [ET1011C] (mii_bus:phy_addr=1:01, id=282f013)
    Sending DHCP requests ..
    PHY: 1:01 - Link is Up - 1000/Full
    ., OK
    IP-Config: Got DHCP answer from 0.0.0.0, my address is 192.168.1.165
    IP-Config: Complete:
         device=eth0, addr=192.168.1.165, mask=255.255.255.0, gw=192.168.1.254,
         host=192.168.1.165, domain=, nis-domain=(none),
         bootserver=0.0.0.0, rootserver=0.0.0.0, rootpath=
    Looking up port of RPC 100003/2 on 0.0.0.0
    rpcbind: server 0.0.0.0 not responding, timed out
    Root-NFS: Unable to get nfsd port number from server, using default
    Looking up port of RPC 100005/1 on 0.0.0.0
    rpcbind: server 0.0.0.0 not responding, timed out
    Root-NFS: Unable to get mountd port number from server, using default
    Root-NFS: Server returned error -5 while mounting /tftpboot/$(nfshost):$(rootpat
    h)
    VFS: Unable to mount root fs via NFS, trying floppy.
    VFS: Cannot open root device "nfs" or unknown-block(2,0)
    Please append a correct "root=" boot option; here are the available partitions:
    0300        39070080 hda driver: ide-gd
      0301        27342598 hda1
      0302        11727450 hda2
    1f00             128 mtdblock0 (driver?)
    1f01            1280 mtdblock1 (driver?)
    1f02            4096 mtdblock2 (driver?)
    1f03          125568 mtdblock3 (driver?)
    Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
    Backtrace:
    [<c00307d0>] (dump_backtrace+0x0/0x114) from [<c030af14>] (dump_stack+0x18/0x1c)

     r7:00008000 r6:c5013000 r5:c0026808 r4:c041e850
    [<c030aefc>] (dump_stack+0x0/0x1c) from [<c030af6c>] (panic+0x54/0x124)
    [<c030af18>] (panic+0x0/0x124) from [<c0008fbc>] (mount_block_root+0x1e0/0x220)
     r3:00000001 r2:c5025e98 r1:c5025f60 r0:c0395ead
    [<c0008ddc>] (mount_block_root+0x0/0x220) from [<c00090c0>] (mount_root+0xc4/0xf
    c)
     r8:00000000 r7:00000000 r6:00000000 r5:00000000 r4:00200000
    [<c0008ffc>] (mount_root+0x0/0xfc) from [<c0009268>] (prepare_namespace+0x170/0x
    1c8)
     r5:c0026808 r4:c041e340
    [<c00090f8>] (prepare_namespace+0x0/0x1c8) from [<c00084bc>] (kernel_init+0xe4/0
    x118)
     r5:00000000 r4:c041e100
    [<c00083d8>] (kernel_init+0x0/0x118) from [<c0045704>] (do_exit+0x0/0x684)
     r5:00000000 r4:00000000

    thanks for your help.

    thierno

     

  • hello,

    my boot from nfs work well,

    i followed this topic

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/99/t/6814.aspx?PageIndex=2

    thanks

    Thierno