This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM335X: am335x

Part Number: PROCESSOR-SDK-AM335X


Tool/software: Linux

Hello,

I am working on Linux 3.12 running on TI AM335x.

Basically I am testing PTP to sync to GPS master.

The Test system is GPS connected to CPU over Ethernet and GPS is configured to send PEER to PEER mode.

I can successfully test using E2E mode there were no issues.

following is the issue when tested with P2P mode.

root@phycore-am335x-1:~# ptp4l -i eth0 -m -P

ptp4l[2103.623]: selected /dev/ptp0 as PTP clock
ptp4l[2103.653]: port 1: INITIALIZING to LISTENING on INITIALIZE
ptp4l[2103.657]: port 0: INITIALIZING to LISTENING on INITIALIZE
ptp4l[2103.724]: port 1: new foreign master 001d7f.fffe.8002f7-1
ptp4l[2103.849]: port 1: received PDELAY_REQ without timestamp
ptp4l[2104.658]: timed out while polling for tx timestamp
ptp4l[2104.659]: increasing tx_timestamp_timeout may correct this issue, but it is likely caused by a driver bug
ptp4l[2104.659]: port 1: send peer delay request failed
ptp4l[2104.659]: port 1: LISTENING to FAULTY on FAULT_DETECTED (FT_UNSPECIFIED)
ptp4l[2120.707]: port 1: FAULTY to LISTENING on FAULT_CLEARED
ptp4l[2120.865]: port 1: received PDELAY_REQ without timestamp
ptp4l[2121.714]: timed out while polling for tx timestamp
ptp4l[2121.715]: increasing tx_timestamp_timeout may correct this issue, but it is likely caused by a driver bug
ptp4l[2121.715]: port 1: send peer delay request failed
ptp4l[2121.715]: port 1: LISTENING to FAULTY on FAULT_DETECTED (FT_UNSPECIFIED)