This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Re: Check the new OMAP-L137 audio application (ARM + DSP)

Other Parts Discussed in Thread: OMAP-L138, TMS320C6748, OMAP-L137, TMS320C6747, ADS1274

Hello, Mariana:

There is a problem in the same category with McBSP of Experimenter board of OMAP-L138/TMS320C6748.

The FSR1 and FSR0 (Receive frame synchronization) signals don't work. The FSR1 signal can be brought

out through the GP0[4] pin of the general I/O Port under the control of register PINMUX1, according to

document SPRUGJ6A.pdf, User's Guide of TMS320C674x/OMAP-L1x Processor McBSP Interface. But the

FSR0 and FSR1 signals can not be brought out. To verify this problem, I first let PINMUX1 = 0x00808080 and

send a logic-one signal (3.3V DC) to GP0[4]. But this GP0[4] pin does not output 3.3V DC when I measure it

with my multimeter (volt/ohm meter), its output is always a constant 0.145V DC.  But the pins of GP0[2] and

GP[6] can output 3.3V DC correctly. This makes me suspect that there may be some silicon error with FRS0

and FSR1 inside DSP OMAP-L138/TMS320C6748.

 

Could you please send a logic-one signal to the GP0[4] pin and see if you are able to measure 3.3V DC

at this pin out?

 

I need to change my DSP from OMAP-L138/TMS320C6748 to OMAP-L137/TMS320C6747 if this is indeed

a silicon problem of the DSP chip. I need the McBSP to interface a 4-channel sigma-delta ADC (TI's ADS1274).

But, OMAP-L137/MTS320C6747 only has McASP but not McBSP. Is it possible to interface ADS1274 with McASP

of OMAP-L137/MTS320C6747?

 

Thank you in advance.

 

WL

 

 

 

 

 

 

 

  • Hi
    Where are you probing the McBSP1 FSX1/FSR1 signals on the experimenter board? If you were probing these signals on the audio expansion connector, then you need to ensure that Switch S7-2 is ON position.I hope this is not the issue with your observation?

     

    Regards

    Mukul