This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: About a restriction on C6748 Power-On/Off Sequence

Part Number: TMS320C6748


Hi Champs,

There is a restriction on C6748 Power-On/Off sequence below.

  LVCMOS supplies operated at 3.3V (DVDD3318_A, DVDD3318_B, or DVDD3318_C)
  never exceed static 1.8V supplies by more than 2 volts.


So, what kind of impact can be considered when the 3.3V exceed the 1.8V by more than 2V?  I'd like to make sure of it.

Regards,
j-breeze