Part Number: 66AK2E05
okay so simple problem. i m not able to fully understand how the flow control is happening in the PA_emac example (Receive setup) i.e. what is the usage of rx_fdq(1-3)_qnum/qmgr
i was under the impression that if for some reason the free descriptors are not enough to handle large number of incoming packets then i can make multiple ques of free descriptors that would run side by side and act as a redundancy for when the descriptors cannot be as fast as the number of incoming packets.
so therefore i created multiple "rxFreeQInfo" as seen in the code below to be used to achieve the idea described above
rxFlowCfg.flowIdNum = CPPI_PARAM_NOT_SPECIFIED;
rxFlowCfg.rx_dest_qmgr = rxQInfo.qMgr;
rxFlowCfg.rx_dest_qnum = rxQInfo.qNum;
rxFlowCfg.rx_desc_type = Cppi_DescType_HOST;
rxFlowCfg.rx_ps_location = Cppi_PSLoc_PS_IN_DESC;
rxFlowCfg.rx_psinfo_present = 1; /* Enable PS info */
rxFlowCfg.rx_error_handling = 1; /* retry on starvation by default */
rxFlowCfg.rx_einfo_present = 1; /* EPIB info present */
rxFlowCfg.rx_dest_tag_lo_sel = 0; /* Disable tagging */
rxFlowCfg.rx_dest_tag_hi_sel = 0;
rxFlowCfg.rx_src_tag_lo_sel = 0;
rxFlowCfg.rx_src_tag_hi_sel = 0;
rxFlowCfg.rx_size_thresh0_en = 0; /* By default, we disable Rx Thresholds */
rxFlowCfg.rx_size_thresh1_en = 0; /* By default, we disable Rx Thresholds */
rxFlowCfg.rx_size_thresh2_en = 0; /* By default, we disable Rx Thresholds */
rxFlowCfg.rx_size_thresh0 = 0x0;
rxFlowCfg.rx_size_thresh1 = 0x0;
rxFlowCfg.rx_size_thresh2 = 0x0;
rxFlowCfg.rx_fdq0_sz0_qmgr = rxFreeQInfo.qMgr; /* Setup the Receive free queue for the flow */
rxFlowCfg.rx_fdq0_sz0_qnum = rxFreeQInfo.qNum;
rxFlowCfg.rx_fdq0_sz1_qnum = 0x0;
rxFlowCfg.rx_fdq0_sz1_qmgr = 0x0;
rxFlowCfg.rx_fdq0_sz2_qnum = 0x0;
rxFlowCfg.rx_fdq0_sz2_qmgr = 0x0;
rxFlowCfg.rx_fdq0_sz3_qnum = 0x0;
rxFlowCfg.rx_fdq0_sz3_qmgr = 0x0;
rxFlowCfg.rx_fdq1_qnum = rxFreeQInfo1.qNum; /* Use the Rx Queue to pick descriptors */
rxFlowCfg.rx_fdq1_qmgr = rxFreeQInfo1.qMgr;
rxFlowCfg.rx_fdq2_qnum = rxFreeQInfo2.qNum; /* Use the Rx Queue to pick descriptors */
rxFlowCfg.rx_fdq2_qmgr = rxFreeQInfo2.qMgr;
rxFlowCfg.rx_fdq3_qnum = rxFreeQInfo3.qNum; /* Use the Rx Queue to pick descriptors */
rxFlowCfg.rx_fdq3_qmgr = rxFreeQInfo3.qMgr;
/* Configure the Rx flow */
if ((gRxFlowHnd = Cppi_configureRxFlow (gCpdmaHnd, &rxFlowCfg, &isAllocated)) == NULL)
{
UART_printf ("Error configuring Rx flow \n");
return -1;
}
is my hypothesis & implementation correct and if so why am i unable to receive data correct had how would and where would i push the used descriptors