Other Parts Discussed in Thread: SYSBIOS, OMAPL138
Hi there, I am using the NDK (ndk_2_25_00_09) with the NSP (nsp_1_10_03_15) in my design and was under the impress that the interrupts used for TX and RX EMAC buffer could be changed if needed.
In the ethdriver.c file I changed the the interrupt number to the following:
#ifdef __TMS470__
#define CORENUM 0
#define RXINT 34
#define TXINT 35
#define EXTMEM 0x80000000
#else
#define CORENUM 1
#define RXINT 10
#define TXINT 11
#define RXTXINTMASK ((1 << RXINT) | (1 << TXINT))
#define EXTMEM 0x80000000
#endif
that is 10 for RXINT and 11 for TXINT. and when I run the design I get the following error:
[C674X_0] Using default MAC address
Using MAC Address: 00-08-ee-03-14-99
rupts: error: could not create RX Hwi!
00000.000 E_alreadyDefined: Hwi already defined: intr# 538976288
ti.sysbios.family.c64p.Hwi: line 194: E_alreadyDefined: Hwi already defined: intr# 6
00000.000 createInterrupts: error: could not create TX Hwi!
00000.000 E_alreadyDefined: Hwi already defined: intr# 538976288
00000.000 EMAC has been started successfully
00000.000 Registeration of the EMAC Successful
00000.000
NC_NetStart: WARNING: Boot thread has not completed!
Network Added: If-1:***.***.***.***
== Start UDP Echo Client Test ==
00000.000 NodeTreeFree: Didn't find right
00000.000 mmFree: Double Free
Could you please, let me know if the interrupt number needs to be changed, elsewhere. Thanks.
Regards,
Mitesh