Part Number: 66AK2G02
Hi Team,
I have a customer using the K2G in a design, and they have some questions:
Refer to my "EMU and Bootmode" drawing for the following questions (only visible to TI employees here--> https://txn.box.com/s/hs216rxicd7homso8r56dlfflt9qmyre), K2G's EMU[2:17] also muxed as bootmode pins for micro SD card boot.
Q1: K2G's BOOTMODE14/EMU16 is for
Boot Acknowledgement:
• 0 = No Boot Acknowledgement expected from MMC
• 1 = Boot Acknowledgement expected, will timeout if not received
What's the setting on EVMK2G when boot from micro SD? Switch the 4-bit DIP on EVMK2G and FPGA, BMC, configures the BOOTMODE[15:00] for me. Since I am able to bootup my own app with micro SD on EVMK2G I would like to know the setting of BOOTMODE14.
Q2: My EMU[19:00] are not buffered and using pullup/pulldown to select BOOTMODE. What is the ideal pullup/pulldown value? 10K or 4.7K?
Q3: For K2G BOOTMODE selection, BOOTMODE[15:00]/EMU[2:17], do I need buffering?
TI wiki says "EMU pins must not be buffered." but I don't know it means EMU[01:00] only or for all EMU pins.
Thank you,
Brian Antheunisse