Part Number: AM3358
Hello,
I tried to load the kernel using ymodem protocol and the download is successful , but i m getting "Wrong image format " error when i run bootm command.
here is a log
U-Boot# loady
## Ready for binary (ymodem) download to 0x80200000 at 115200 bps...
CModem - CRC mode, 33679(SOH)/0(STX)/0(CAN) packets, 3 retries
## Total Size = 0x0041c660 = 4310624 Bytes
U-Boot# bootm 0x80200000
Wrong Image Format for bootm command
ERROR: can't get kernel image!
am i missing something ?
Thanks