Other Parts Discussed in Thread: PMP
Tool/software: Linux
Hello.
I have some questions about HDMI at AM389x.
Thank you for your patience. I'm not a english native speaker. But I hope that you may understand what i say very well.
1. Issue
I use the board based on AM392x. Some boards are blacked out at the LCD panel. So I want to figure out the reason and find the solving solution.
Turn on the board and keep on 2 ~ 6 hour over, The LCD panel turn to black screen(There is no display nothing).
That is not fixed occur time. Every time differ.
2. Environments
1) OS: Linux (kernel 2.6)
2) LCD program: nano-X (ver 20110730) & FLTK (ver 1.3.3)
3) Display output: HDMI
4) Connection
- Board - Scaler board - LCD panel
- Use HDMI and USB cable.
- HDMI used for display screen, USB used to receive touch input from LCD.
3. Checked information
1) Compared scoping sign data normal and un-normal state.
- Scoping point: HDMI data line at scaler board.
- In un-normal state, I checked the homogeneous sign. So expect that there is no data or received “0” .
2) Checked HDMI register value.
- There is no differ.
- For more detail information, check upload files.
3) I reset HDMI by change the reset register. "No signal Input" displayed at LCD around 10 sec. But that string disappeared and show blacked out screen same.
4) We found some log form "dmesg" and find out timeout.
|
Hdmi: first hpd register device crongfb_drv Ver 0.8.2.0 OK (major = 201) CMEMK module: built on Jan 7 2013 at 17:27:04 Reference Linux version 2.6.37 File /home/v10528/workspace_svn/crong/eLinux/linuxutils_3_22_00_02/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c Allocated heap buffer 0x98000000 of size 0x30000000 Cmemk initialized Syslink-2_10_03_20 / packages / ti / syslink / utils / ti-syslink-2_10_03_20-r4j / ti-sysm-none-linux-gnueabi / Hlos / knl / Linux /../../../../../../ ti / syslink / ipc / hlos / knl / NameServerRemoteNotify.c: ((status == NameServer_S_SUCCESS) = NameServer_E_NOTFOUND)): failed Syslink-2_10_03_20 / packages / ti / syslink / utils / ti-syslink-2_10_03_20-r4j / ti-sysm-none-linux-gnueabi / Hlos / knl / Linux /../../../../../../ ti / syslink / ipc / hlos / knl / NameServerRemoteNotify.c: ((status == NameServer_S_SUCCESS) = NameServer_E_NOTFOUND)): failed Syslink-2_10_03_20 / packages / ti / syslink / utils / ti-syslink-2_10_03_20-r4j / ti-sysm-none-linux-gnueabi / Hlos / knl / Linux /../../../../../../ ti / syslink / ipc / hlos / knl / NameServerRemoteNotify.c: ((status == NameServer_S_SUCCESS) = NameServer_E_NOTFOUND)): failed VPSS_FVID2: contrl event 0x6 timeout Ti81xxfb ti81xxfb: failed to stop. |
4. Questions
1) Have you heard about this issue? Can you give me the answer?
2) What is the reason that occur VPSS_FVID2 time out, How to solve the problem?
3) What reason can occur VPSS_FVID2 timeout error?
4) What HW parmeters can give affect to VPSSS output data?
5) Is there register for checking VPSS output state?
6) How to reset VPSS or VPSS output data?
Thank you.