What are the advantages or disadvantages to generating the 32KHz clock internally (sys_boot7 tied to VDDSHV) as opposed to using an external 32KHz oscillator (sys_boot7 tied to RET)?
Do I lose functionality by generating this clock internally?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What are the advantages or disadvantages to generating the 32KHz clock internally (sys_boot7 tied to VDDSHV) as opposed to using an external 32KHz oscillator (sys_boot7 tied to RET)?
Do I lose functionality by generating this clock internally?
If
u are using internal 32k clk generation, this would help u reduce ur system
cost as u can eliminate additional 32k cystal frm board. As 32k required for
device operation would be generated internally frm 26 MHz clk.
Disadvantage of using this option would be that you can't turn HF clk when in off
mode (deep sleep mode) lowest power state at system level. you would still be able to put device in OFF mode but to further reduce power you won't be able to turn OFF HF crystal (26 MHz) on board.
Hence based on product need you would have option to choose based on system requirements.
Thanks and Best Regards,
Vaibhav Desai
Hi Ken,
An internally generated clock only supports 32.5 kHz not 32.768 kHz so it can't be used for real time clock.
advantages
- reduce the BOM cost of a 32KHz oscillator
disadvantages
- can't be used for real time clock
Regards,
Kazunobu Shin