This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

unable to locate documenation (e.g. SPRUGA3.pdf, SPRUG99.pdf)



Arent these documents online somewhere ?

These are mentioned for the dm6467 in DVSDK_Contents, including :

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

DM6467

SPRUG85.pdf

 

 

- LSP 2.00 DaVinci Linux Consumer-IR Driver

SPRUG97.pdf

 

 

- LSP 2.0 DaVinci Linux PCI Slave Driver

SPRUG99.pdf

 

 

- LSP 2.0 DaVinci Linux VPIF Capture Video Driver

SPRUGA0.pdf

 

 

- LSP 2.00 DaVinci Linux VPIF Display Video Driver

SPRUGA1.pdf

 

 

- LSP 2.00 DaVinci Linux PCI Boot Driver

SPRUGA2.pdf

 

 

- LSP 2.00 DaVinci Linux TSIF Driver

SPRUGA3.pdf

 

 

- LSP 2.00 DaVinci Linux Video VDCE Driver

  • Hi,

    AFAIK, these documents should be present in the DVSDK package itself in the docs folder.

    So, rather than searching them online, try the path

    dvsdk_X_XX_XX_XX \ PSP_XX_XX_XX_XXX \ docs \ dm6467 \

    Regards,

    Sid