This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Using PRU UART as standard UART under Linux

Part Number: AM5728

Team,

Our processor SDK doesn't support using the PRU-UART as additional UART in Linux. But could a customer implement this themselves, without running any UART firmware on the PRU? I know interrupt handling is not supported, but couldnt's it be enough to directly access the PRU UART registers from the Cortex A15?

My customer is using all PRUs as additional Ethernet ports, so there is already Ethernet firmware running on the PRUs. It would be good to be able to use the PRU-UART pins as additional UART.

Thanks,
  Robert