Other Parts Discussed in Thread: AM5728
Hi, sir:
I am using mcasp of am5728. Now I want to change the default channels number which equals to 2.
int channels = params_channels(params); // here I printk the value of channels, this code is in davinci-mcasp.c
I truely believed that when I use alsa framework, I only need to call the function snd_pcm_set_params to set the channels.
But when I do so , I still get the same value of 2 like before. Would you please tell me why? Thanks a lot!
My pragram is as below:
/*
* This extra small demo sends a random samples to your speakers.
*/
#include <alsa/asoundlib.h>
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <sched.h>
#include <errno.h>
#include <getopt.h>
#include <math.h>
static char *device = "default"; /* playback device */
snd_output_t *output = NULL;
unsigned char buffer[1*1024]; /* some random data */
//unsigned short int buffer[1*1024]; /* some random data */
int main(void)
{
int err;
unsigned int i;
snd_pcm_t *handle;
//snd_pcm_hw_params_t *hwparams;
snd_pcm_sframes_t frames;
//int channels = 4;
printf("size of buffer is %d\n", sizeof(buffer));
for (i = 0; i < sizeof(buffer); i++)
//buffer[i] = random() & 0xff;
//buffer[i] = 0xff;
buffer[i] = i;
if ((err = snd_pcm_open(&handle, device, SND_PCM_STREAM_PLAYBACK, 0)) < 0) {
printf("Playback open error: %s\n", snd_strerror(err));
exit(EXIT_FAILURE);
}
//snd_pcm_hw_params_alloca(&hwparams);
//snd_pcm_hw_params_set_channels(handle, hwparams, channels);
if ((err = snd_pcm_set_params(handle,
//SND_PCM_FORMAT_U8,
SND_PCM_FORMAT_U16,
SND_PCM_ACCESS_RW_INTERLEAVED,
16, // channels
48000,
1,
500000)) < 0) { /* 0.5sec */
printf("Playback open error: %s\n", snd_strerror(err));
exit(EXIT_FAILURE);
}
//for (i = 0; i < 16; i++) {
//while(1){
// frames = snd_pcm_writei(handle, buffer, sizeof(buffer));
// //printf("frames = %d\n", frames);
// if (frames < 0)
// frames = snd_pcm_recover(handle, frames, 0);
// if (frames < 0) {
// printf("snd_pcm_writei failed: %s\n", snd_strerror(frames));
// break;
// }
// if (frames > 0 && frames < (long)sizeof(buffer))
// printf("Short write (expected %li, wrote %li)\n", (long)sizeof(buffer), frames);
// //snd_pcm_drain(handle);
//}
snd_pcm_close(handle);
return 0;
}