This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Creating project for Profibus Master

Part Number: AM5728
Other Parts Discussed in Thread: PROFIBUS

Hi, Everyone

I have a question about PROFIBUS Master of PRU-ICSS-PROFIBUS-MASTER for AM572x.

I try to Generating Project files in Users guide.
and set setupEnv.bat and run.
but it got error of No XDCtools.

I use CCSv6.1.2. and pdk_am57x_1_0_2

and I watched projectCreate.bat on defalt below:

:: Set XDC Tools Version which is to be used while creating the project

set "XDC_TOOLS_VERSION=3.32.00.36_core"

Actually xdctools is not released this version of 3.32.00.36_core.
and I changed this version.
but It still get error.

Can you help me ?

Best Regards
Hiroyasu