This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6672: How to clear I2C Bus hang condition

Part Number: TMS320C6672


In sprz335h (TMS320C6672 Silicon Errata) Usage Note 6 describes how to clear a I2C bus hang that can occur when a master is reset in the middle of a I2C transaction.

It is said there that "An I2C master must generate up to 9 clock cycles ..." and so on,

but the details of such an impelmentation using the TMS320C6672 as master are not described.

Questions:

Is it possible at all implementing such an I2C bus clear using the TMS320C6672 as master (I found no hints using SDA and SCL as gpio)?

Or are there additional hardware design measures neccesarry to accomplish such a task with the TMS320C6672?

Excerpt from sprz335h (TMS320C6672 Silicon Errata)

Usage Note 6 I2C Bus Hang After Master Reset Usage Note
Revision(s) Affected: 1.0, 2.0
Details: It is generally known that the I2C bus can hang if an I2C master is removed from the bus
in the middle of a data read. This can occur because the I2C protocol does not mandate
a minimum clock rate. Therefore, if a master is reset in the middle of a read while a
slave is driving the data line low, the slave will continue driving the data line low while it
waits for the next clock edge. This prevents bus masters from initiating transfers. If this
condition is detected, the following three steps will clear the bus hang condition:
1. An I2C master must generate up to 9 clock cycles.
2. After each clock cycle, the data pin must be observed to determine whether it has
gone high while the clock is high.
3. As soon as the data pin is observed high, the master can initiate a start condition.

  • Hi Juergen,

    Not sure about RTOS implementation on this, however in linux kernels (implementation is from kernel 4.4.32) 

    /*
     * TI DAVINCI I2C adapter driver.
     *
     * Copyright (C) 2006 Texas Instruments.
     * Copyright (C) 2007 MontaVista Software Inc.
     *
     * Updated by Vinod & Sudhakar Feb 2005
     *
     * ----------------------------------------------------------------------------
     *
     * This program is free software; you can redistribute it and/or modify
     * it under the terms of the GNU General Public License as published by
     * the Free Software Foundation; either version 2 of the License, or
     * (at your option) any later version.
     *
     * This program is distributed in the hope that it will be useful,
     * but WITHOUT ANY WARRANTY; without even the implied warranty of
     * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
     * GNU General Public License for more details.
     * ----------------------------------------------------------------------------
     *
     */
    #include <linux/kernel.h>
    #include <linux/module.h>
    #include <linux/delay.h>
    #include <linux/i2c.h>
    #include <linux/clk.h>
    #include <linux/errno.h>
    #include <linux/sched.h>
    #include <linux/err.h>
    #include <linux/interrupt.h>
    #include <linux/platform_device.h>
    #include <linux/io.h>
    #include <linux/slab.h>
    #include <linux/cpufreq.h>
    #include <linux/gpio.h>
    #include <linux/of_device.h>
    #include <linux/platform_data/i2c-davinci.h>
    
    /* ----- global defines ----------------------------------------------- */
    
    #define DAVINCI_I2C_TIMEOUT	(1*HZ)
    #define DAVINCI_I2C_MAX_TRIES	2
    #define DAVINCI_I2C_OWN_ADDRESS	0x08
    #define I2C_DAVINCI_INTR_ALL    (DAVINCI_I2C_IMR_SCD | \
    				 DAVINCI_I2C_IMR_ARDY | \
    				 DAVINCI_I2C_IMR_NACK | \
    				 DAVINCI_I2C_IMR_AL)
    
    #define DAVINCI_I2C_OAR_REG	0x00
    #define DAVINCI_I2C_IMR_REG	0x04
    #define DAVINCI_I2C_STR_REG	0x08
    #define DAVINCI_I2C_CLKL_REG	0x0c
    #define DAVINCI_I2C_CLKH_REG	0x10
    #define DAVINCI_I2C_CNT_REG	0x14
    #define DAVINCI_I2C_DRR_REG	0x18
    #define DAVINCI_I2C_SAR_REG	0x1c
    #define DAVINCI_I2C_DXR_REG	0x20
    #define DAVINCI_I2C_MDR_REG	0x24
    #define DAVINCI_I2C_IVR_REG	0x28
    #define DAVINCI_I2C_EMDR_REG	0x2c
    #define DAVINCI_I2C_PSC_REG	0x30
    #define DAVINCI_I2C_FUNC_REG	0x48
    #define DAVINCI_I2C_DIR_REG	0x4c
    #define DAVINCI_I2C_DIN_REG	0x50
    #define DAVINCI_I2C_DOUT_REG	0x54
    #define DAVINCI_I2C_DSET_REG	0x58
    #define DAVINCI_I2C_DCLR_REG	0x5c
    
    #define DAVINCI_I2C_IVR_AAS	0x07
    #define DAVINCI_I2C_IVR_SCD	0x06
    #define DAVINCI_I2C_IVR_XRDY	0x05
    #define DAVINCI_I2C_IVR_RDR	0x04
    #define DAVINCI_I2C_IVR_ARDY	0x03
    #define DAVINCI_I2C_IVR_NACK	0x02
    #define DAVINCI_I2C_IVR_AL	0x01
    
    #define DAVINCI_I2C_STR_BB	BIT(12)
    #define DAVINCI_I2C_STR_RSFULL	BIT(11)
    #define DAVINCI_I2C_STR_SCD	BIT(5)
    #define DAVINCI_I2C_STR_ARDY	BIT(2)
    #define DAVINCI_I2C_STR_NACK	BIT(1)
    #define DAVINCI_I2C_STR_AL	BIT(0)
    
    #define DAVINCI_I2C_MDR_NACK	BIT(15)
    #define DAVINCI_I2C_MDR_STT	BIT(13)
    #define DAVINCI_I2C_MDR_STP	BIT(11)
    #define DAVINCI_I2C_MDR_MST	BIT(10)
    #define DAVINCI_I2C_MDR_TRX	BIT(9)
    #define DAVINCI_I2C_MDR_XA	BIT(8)
    #define DAVINCI_I2C_MDR_RM	BIT(7)
    #define DAVINCI_I2C_MDR_IRS	BIT(5)
    
    #define DAVINCI_I2C_IMR_AAS	BIT(6)
    #define DAVINCI_I2C_IMR_SCD	BIT(5)
    #define DAVINCI_I2C_IMR_XRDY	BIT(4)
    #define DAVINCI_I2C_IMR_RRDY	BIT(3)
    #define DAVINCI_I2C_IMR_ARDY	BIT(2)
    #define DAVINCI_I2C_IMR_NACK	BIT(1)
    #define DAVINCI_I2C_IMR_AL	BIT(0)
    
    /* set SDA and SCL as GPIO */
    #define DAVINCI_I2C_FUNC_PFUNC0	BIT(0)
    
    /* set SCL as output when used as GPIO*/
    #define DAVINCI_I2C_DIR_PDIR0	BIT(0)
    /* set SDA as output when used as GPIO*/
    #define DAVINCI_I2C_DIR_PDIR1	BIT(1)
    
    /* read SCL GPIO level */
    #define DAVINCI_I2C_DIN_PDIN0 BIT(0)
    /* read SDA GPIO level */
    #define DAVINCI_I2C_DIN_PDIN1 BIT(1)
    
    /*set the SCL GPIO high */
    #define DAVINCI_I2C_DSET_PDSET0	BIT(0)
    /*set the SDA GPIO high */
    #define DAVINCI_I2C_DSET_PDSET1	BIT(1)
    
    /* set the SCL GPIO low */
    #define DAVINCI_I2C_DCLR_PDCLR0	BIT(0)
    /* set the SDA GPIO low */
    #define DAVINCI_I2C_DCLR_PDCLR1	BIT(1)
    
    struct davinci_i2c_dev {
    	struct device           *dev;
    	void __iomem		*base;
    	struct completion	cmd_complete;
    	struct clk              *clk;
    	int			cmd_err;
    	u8			*buf;
    	size_t			buf_len;
    	int			irq;
    	int			stop;
    	u8			terminate;
    	struct i2c_adapter	adapter;
    #ifdef CONFIG_CPU_FREQ
    	struct completion	xfr_complete;
    	struct notifier_block	freq_transition;
    #endif
    	struct davinci_i2c_platform_data *pdata;
    };
    
    /* default platform data to use if not supplied in the platform_device */
    static struct davinci_i2c_platform_data davinci_i2c_platform_data_default = {
    	.bus_freq	= 100,
    	.bus_delay	= 0,
    };
    
    static inline void davinci_i2c_write_reg(struct davinci_i2c_dev *i2c_dev,
    					 int reg, u16 val)
    {
    	writew_relaxed(val, i2c_dev->base + reg);
    }
    
    static inline u16 davinci_i2c_read_reg(struct davinci_i2c_dev *i2c_dev, int reg)
    {
    	return readw_relaxed(i2c_dev->base + reg);
    }
    
    static inline void davinci_i2c_reset_ctrl(struct davinci_i2c_dev *i2c_dev,
    								int val)
    {
    	u16 w;
    
    	w = davinci_i2c_read_reg(i2c_dev, DAVINCI_I2C_MDR_REG);
    	if (!val)	/* put I2C into reset */
    		w &= ~DAVINCI_I2C_MDR_IRS;
    	else		/* take I2C out of reset */
    		w |= DAVINCI_I2C_MDR_IRS;
    
    	davinci_i2c_write_reg(i2c_dev, DAVINCI_I2C_MDR_REG, w);
    }
    
    static void i2c_davinci_calc_clk_dividers(struct davinci_i2c_dev *dev)
    {
    	struct davinci_i2c_platform_data *pdata = dev->pdata;
    	u16 psc;
    	u32 clk;
    	u32 d;
    	u32 clkh;
    	u32 clkl;
    	u32 input_clock = clk_get_rate(dev->clk);
    	struct device_node *of_node = dev->dev->of_node;
    
    	/* NOTE: I2C Clock divider programming info
    	 * As per I2C specs the following formulas provide prescaler
    	 * and low/high divider values
    	 * input clk --> PSC Div -----------> ICCL/H Div --> output clock
    	 *                       module clk
    	 *
    	 * output clk = module clk / (PSC + 1) [ (ICCL + d) + (ICCH + d) ]
    	 *
    	 * Thus,
    	 * (ICCL + ICCH) = clk = (input clk / ((psc +1) * output clk)) - 2d;
    	 *
    	 * where if PSC == 0, d = 7,
    	 *       if PSC == 1, d = 6
    	 *       if PSC > 1 , d = 5
    	 *
    	 * Note:
    	 * d is always 6 on Keystone I2C controller
    	 */
    
    	/*
    	 * Both Davinci and current Keystone User Guides recommend a value
    	 * between 7MHz and 12MHz. In reality 7MHz module clock doesn't
    	 * always produce enough margin between SDA and SCL transitions.
    	 * Measurements show that the higher the module clock is, the
    	 * bigger is the margin, providing more reliable communication.
    	 * So we better target for 12MHz.
    	 */
    	psc = (input_clock / 12000000) - 1;
    	if ((input_clock / (psc + 1)) > 12000000)
    		psc++;	/* better to run under spec than over */
    	d = (psc >= 2) ? 5 : 7 - psc;
    
    	if (of_node && of_device_is_compatible(of_node, "ti,keystone-i2c"))
    		d = 6;
    
    	clk = ((input_clock / (psc + 1)) / (pdata->bus_freq * 1000));
    	/* Avoid driving the bus too fast because of rounding errors above */
    	if (input_clock / (psc + 1) / clk > pdata->bus_freq * 1000)
    		clk++;
    	/*
    	 * According to I2C-BUS Spec 2.1, in FAST-MODE LOW period should be at
    	 * least 1.3uS, which is not the case with 50% duty cycle. Driving HIGH
    	 * to LOW ratio as 1 to 2 is more safe.
    	 */
    	if (pdata->bus_freq > 100)
    		clkl = (clk << 1) / 3;
    	else
    		clkl = (clk >> 1);
    	/*
    	 * It's not always possible to have 1 to 2 ratio when d=7, so fall back
    	 * to minimal possible clkh in this case.
    	 */
    	if (clk >= clkl + d) {
    		clkh = clk - clkl - d;
    		clkl -= d;
    	} else {
    		clkh = 0;
    		clkl = clk - (d << 1);
    	}
    
    	davinci_i2c_write_reg(dev, DAVINCI_I2C_PSC_REG, psc);
    	davinci_i2c_write_reg(dev, DAVINCI_I2C_CLKH_REG, clkh);
    	davinci_i2c_write_reg(dev, DAVINCI_I2C_CLKL_REG, clkl);
    
    	dev_dbg(dev->dev, "input_clock = %d, CLK = %d\n", input_clock, clk);
    }
    
    /*
     * This function configures I2C and brings I2C out of reset.
     * This function is called during I2C init function. This function
     * also gets called if I2C encounters any errors.
     */
    static int i2c_davinci_init(struct davinci_i2c_dev *dev)
    {
    	struct davinci_i2c_platform_data *pdata = dev->pdata;
    
    	/* put I2C into reset */
    	davinci_i2c_reset_ctrl(dev, 0);
    
    	/* compute clock dividers */
    	i2c_davinci_calc_clk_dividers(dev);
    
    	/* Respond at reserved "SMBus Host" slave address" (and zero);
    	 * we seem to have no option to not respond...
    	 */
    	davinci_i2c_write_reg(dev, DAVINCI_I2C_OAR_REG, DAVINCI_I2C_OWN_ADDRESS);
    
    	dev_dbg(dev->dev, "PSC  = %d\n",
    		davinci_i2c_read_reg(dev, DAVINCI_I2C_PSC_REG));
    	dev_dbg(dev->dev, "CLKL = %d\n",
    		davinci_i2c_read_reg(dev, DAVINCI_I2C_CLKL_REG));
    	dev_dbg(dev->dev, "CLKH = %d\n",
    		davinci_i2c_read_reg(dev, DAVINCI_I2C_CLKH_REG));
    	dev_dbg(dev->dev, "bus_freq = %dkHz, bus_delay = %d\n",
    		pdata->bus_freq, pdata->bus_delay);
    
    
    	/* Take the I2C module out of reset: */
    	davinci_i2c_reset_ctrl(dev, 1);
    
    	/* Enable interrupts */
    	davinci_i2c_write_reg(dev, DAVINCI_I2C_IMR_REG, I2C_DAVINCI_INTR_ALL);
    
    	return 0;
    }
    
    /*
     * This routine does i2c bus recovery by using i2c_generic_gpio_recovery
     * which is provided by I2C Bus recovery infrastructure.
     */
    static void davinci_i2c_prepare_recovery(struct i2c_adapter *adap)
    {
    	struct davinci_i2c_dev *dev = i2c_get_adapdata(adap);
    
    	/* Disable interrupts */
    	davinci_i2c_write_reg(dev, DAVINCI_I2C_IMR_REG, 0);
    
    	/* put I2C into reset */
    	davinci_i2c_reset_ctrl(dev, 0);
    }
    
    static void davinci_i2c_unprepare_recovery(struct i2c_adapter *adap)
    {
    	struct davinci_i2c_dev *dev = i2c_get_adapdata(adap);
    
    	i2c_davinci_init(dev);
    }
    
    static struct i2c_bus_recovery_info davinci_i2c_gpio_recovery_info = {
    	.recover_bus = i2c_generic_gpio_recovery,
    	.prepare_recovery = davinci_i2c_prepare_recovery,
    	.unprepare_recovery = davinci_i2c_unprepare_recovery,
    };
    
    static void davinci_i2c_set_scl(struct i2c_adapter *adap, int val)
    {
    	struct davinci_i2c_dev *dev = i2c_get_adapdata(adap);
    
    	if (val)
    		davinci_i2c_write_reg(dev, DAVINCI_I2C_DSET_REG,
    				      DAVINCI_I2C_DSET_PDSET0);
    	else
    		davinci_i2c_write_reg(dev, DAVINCI_I2C_DCLR_REG,
    				      DAVINCI_I2C_DCLR_PDCLR0);
    }
    
    static int davinci_i2c_get_scl(struct i2c_adapter *adap)
    {
    	struct davinci_i2c_dev *dev = i2c_get_adapdata(adap);
    	int val;
    
    	/* read the state of SCL */
    	val = davinci_i2c_read_reg(dev, DAVINCI_I2C_DIN_REG);
    	return val & DAVINCI_I2C_DIN_PDIN0;
    }
    
    static int davinci_i2c_get_sda(struct i2c_adapter *adap)
    {
    	struct davinci_i2c_dev *dev = i2c_get_adapdata(adap);
    	int val;
    
    	/* read the state of SDA */
    	val = davinci_i2c_read_reg(dev, DAVINCI_I2C_DIN_REG);
    	return val & DAVINCI_I2C_DIN_PDIN1;
    }
    
    static void davinci_i2c_scl_prepare_recovery(struct i2c_adapter *adap)
    {
    	struct davinci_i2c_dev *dev = i2c_get_adapdata(adap);
    
    	davinci_i2c_prepare_recovery(adap);
    
    	/* SCL output, SDA input */
    	davinci_i2c_write_reg(dev, DAVINCI_I2C_DIR_REG, DAVINCI_I2C_DIR_PDIR0);
    
    	/* change to GPIO mode */
    	davinci_i2c_write_reg(dev, DAVINCI_I2C_FUNC_REG,
    			      DAVINCI_I2C_FUNC_PFUNC0);
    }
    
    static void davinci_i2c_scl_unprepare_recovery(struct i2c_adapter *adap)
    {
    	struct davinci_i2c_dev *dev = i2c_get_adapdata(adap);
    
    	/* change back to I2C mode */
    	davinci_i2c_write_reg(dev, DAVINCI_I2C_FUNC_REG, 0);
    
    	davinci_i2c_unprepare_recovery(adap);
    }
    
    static struct i2c_bus_recovery_info davinci_i2c_scl_recovery_info = {
    	.recover_bus = i2c_generic_scl_recovery,
    	.set_scl = davinci_i2c_set_scl,
    	.get_scl = davinci_i2c_get_scl,
    	.get_sda = davinci_i2c_get_sda,
    	.prepare_recovery = davinci_i2c_scl_prepare_recovery,
    	.unprepare_recovery = davinci_i2c_scl_unprepare_recovery,
    };
    
    /*
     * Waiting for bus not busy
     */
    static int i2c_davinci_wait_bus_not_busy(struct davinci_i2c_dev *dev)
    {
    	unsigned long timeout = jiffies + dev->adapter.timeout;
    
    	do {
    		if (!(davinci_i2c_read_reg(dev, DAVINCI_I2C_STR_REG) & DAVINCI_I2C_STR_BB))
    			return 0;
    		schedule_timeout_uninterruptible(1);
    	} while (time_before_eq(jiffies, timeout));
    
    	dev_warn(dev->dev, "timeout waiting for bus ready\n");
    	i2c_recover_bus(&dev->adapter);
    
    	/*
    	 * if bus is still "busy" here, it's most probably a HW problem like
    	 * short-circuit
    	 */
    	if (davinci_i2c_read_reg(dev, DAVINCI_I2C_STR_REG) & DAVINCI_I2C_STR_BB)
    		return -EIO;
    
    	return 0;
    }
    
    /*
     * Low level master read/write transaction. This function is called
     * from i2c_davinci_xfer.
     */
    static int
    i2c_davinci_xfer_msg(struct i2c_adapter *adap, struct i2c_msg *msg, int stop)
    {
    	struct davinci_i2c_dev *dev = i2c_get_adapdata(adap);
    	struct davinci_i2c_platform_data *pdata = dev->pdata;
    	u32 flag;
    	u16 w;
    	unsigned long time_left;
    
    	if (msg->addr == DAVINCI_I2C_OWN_ADDRESS) {
    		dev_warn(dev->dev, "transfer to own address aborted\n");
    		return -EADDRNOTAVAIL;
    	}
    
    	/* Introduce a delay, required for some boards (e.g Davinci EVM) */
    	if (pdata->bus_delay)
    		udelay(pdata->bus_delay);
    
    	/* set the slave address */
    	davinci_i2c_write_reg(dev, DAVINCI_I2C_SAR_REG, msg->addr);
    
    	dev->buf = msg->buf;
    	dev->buf_len = msg->len;
    	dev->stop = stop;
    
    	davinci_i2c_write_reg(dev, DAVINCI_I2C_CNT_REG, dev->buf_len);
    
    	reinit_completion(&dev->cmd_complete);
    	dev->cmd_err = 0;
    
    	/* Take I2C out of reset and configure it as master */
    	flag = DAVINCI_I2C_MDR_IRS | DAVINCI_I2C_MDR_MST;
    
    	/* if the slave address is ten bit address, enable XA bit */
    	if (msg->flags & I2C_M_TEN)
    		flag |= DAVINCI_I2C_MDR_XA;
    	if (!(msg->flags & I2C_M_RD))
    		flag |= DAVINCI_I2C_MDR_TRX;
    	if (msg->len == 0)
    		flag |= DAVINCI_I2C_MDR_RM;
    
    	/* Enable receive or transmit interrupts */
    	w = davinci_i2c_read_reg(dev, DAVINCI_I2C_IMR_REG);
    	if (msg->flags & I2C_M_RD)
    		w |= DAVINCI_I2C_IMR_RRDY;
    	else
    		w |= DAVINCI_I2C_IMR_XRDY;
    	davinci_i2c_write_reg(dev, DAVINCI_I2C_IMR_REG, w);
    
    	dev->terminate = 0;
    
    	/*
    	 * Write mode register first as needed for correct behaviour
    	 * on OMAP-L138, but don't set STT yet to avoid a race with XRDY
    	 * occurring before we have loaded DXR
    	 */
    	davinci_i2c_write_reg(dev, DAVINCI_I2C_MDR_REG, flag);
    
    	/*
    	 * First byte should be set here, not after interrupt,
    	 * because transmit-data-ready interrupt can come before
    	 * NACK-interrupt during sending of previous message and
    	 * ICDXR may have wrong data
    	 * It also saves us one interrupt, slightly faster
    	 */
    	if ((!(msg->flags & I2C_M_RD)) && dev->buf_len) {
    		davinci_i2c_write_reg(dev, DAVINCI_I2C_DXR_REG, *dev->buf++);
    		dev->buf_len--;
    	}
    
    	/* Set STT to begin transmit now DXR is loaded */
    	flag |= DAVINCI_I2C_MDR_STT;
    	if (stop && msg->len != 0)
    		flag |= DAVINCI_I2C_MDR_STP;
    	davinci_i2c_write_reg(dev, DAVINCI_I2C_MDR_REG, flag);
    
    	time_left = wait_for_completion_timeout(&dev->cmd_complete,
    						dev->adapter.timeout);
    	if (!time_left) {
    		dev_err(dev->dev, "controller timed out\n");
    		i2c_recover_bus(adap);
    		dev->buf_len = 0;
    		return -ETIMEDOUT;
    	}
    	if (dev->buf_len) {
    		/* This should be 0 if all bytes were transferred
    		 * or dev->cmd_err denotes an error.
    		 */
    		dev_err(dev->dev, "abnormal termination buf_len=%i\n",
    			dev->buf_len);
    		dev->terminate = 1;
    		wmb();
    		dev->buf_len = 0;
    		return -EREMOTEIO;
    	}
    
    	/* no error */
    	if (likely(!dev->cmd_err))
    		return msg->len;
    
    	/* We have an error */
    	if (dev->cmd_err & DAVINCI_I2C_STR_AL) {
    		i2c_davinci_init(dev);
    		return -EIO;
    	}
    
    	if (dev->cmd_err & DAVINCI_I2C_STR_NACK) {
    		if (msg->flags & I2C_M_IGNORE_NAK)
    			return msg->len;
    		w = davinci_i2c_read_reg(dev, DAVINCI_I2C_MDR_REG);
    		w |= DAVINCI_I2C_MDR_STP;
    		davinci_i2c_write_reg(dev, DAVINCI_I2C_MDR_REG, w);
    		return -EREMOTEIO;
    	}
    	return -EIO;
    }
    
    /*
     * Prepare controller for a transaction and call i2c_davinci_xfer_msg
     */
    static int
    i2c_davinci_xfer(struct i2c_adapter *adap, struct i2c_msg msgs[], int num)
    {
    	struct davinci_i2c_dev *dev = i2c_get_adapdata(adap);
    	int i;
    	int ret;
    
    	dev_dbg(dev->dev, "%s: msgs: %d\n", __func__, num);
    
    	ret = i2c_davinci_wait_bus_not_busy(dev);
    	if (ret < 0) {
    		dev_warn(dev->dev, "timeout waiting for bus ready\n");
    		return ret;
    	}
    
    	for (i = 0; i < num; i++) {
    		ret = i2c_davinci_xfer_msg(adap, &msgs[i], (i == (num - 1)));
    		dev_dbg(dev->dev, "%s [%d/%d] ret: %d\n", __func__, i + 1, num,
    			ret);
    		if (ret < 0)
    			return ret;
    	}
    
    #ifdef CONFIG_CPU_FREQ
    	complete(&dev->xfr_complete);
    #endif
    
    	return num;
    }
    
    static u32 i2c_davinci_func(struct i2c_adapter *adap)
    {
    	return I2C_FUNC_I2C | I2C_FUNC_SMBUS_EMUL;
    }
    
    static void terminate_read(struct davinci_i2c_dev *dev)
    {
    	u16 w = davinci_i2c_read_reg(dev, DAVINCI_I2C_MDR_REG);
    	w |= DAVINCI_I2C_MDR_NACK;
    	davinci_i2c_write_reg(dev, DAVINCI_I2C_MDR_REG, w);
    
    	/* Throw away data */
    	davinci_i2c_read_reg(dev, DAVINCI_I2C_DRR_REG);
    	if (!dev->terminate)
    		dev_err(dev->dev, "RDR IRQ while no data requested\n");
    }
    static void terminate_write(struct davinci_i2c_dev *dev)
    {
    	u16 w = davinci_i2c_read_reg(dev, DAVINCI_I2C_MDR_REG);
    	w |= DAVINCI_I2C_MDR_RM | DAVINCI_I2C_MDR_STP;
    	davinci_i2c_write_reg(dev, DAVINCI_I2C_MDR_REG, w);
    
    	if (!dev->terminate)
    		dev_dbg(dev->dev, "TDR IRQ while no data to send\n");
    }
    
    /*
     * Interrupt service routine. This gets called whenever an I2C interrupt
     * occurs.
     */
    static irqreturn_t i2c_davinci_isr(int this_irq, void *dev_id)
    {
    	struct davinci_i2c_dev *dev = dev_id;
    	u32 stat;
    	int count = 0;
    	u16 w;
    
    	while ((stat = davinci_i2c_read_reg(dev, DAVINCI_I2C_IVR_REG))) {
    		dev_dbg(dev->dev, "%s: stat=0x%x\n", __func__, stat);
    		if (count++ == 100) {
    			dev_warn(dev->dev, "Too much work in one IRQ\n");
    			break;
    		}
    
    		switch (stat) {
    		case DAVINCI_I2C_IVR_AL:
    			/* Arbitration lost, must retry */
    			dev->cmd_err |= DAVINCI_I2C_STR_AL;
    			dev->buf_len = 0;
    			complete(&dev->cmd_complete);
    			break;
    
    		case DAVINCI_I2C_IVR_NACK:
    			dev->cmd_err |= DAVINCI_I2C_STR_NACK;
    			dev->buf_len = 0;
    			complete(&dev->cmd_complete);
    			break;
    
    		case DAVINCI_I2C_IVR_ARDY:
    			davinci_i2c_write_reg(dev,
    				DAVINCI_I2C_STR_REG, DAVINCI_I2C_STR_ARDY);
    			if (((dev->buf_len == 0) && (dev->stop != 0)) ||
    			    (dev->cmd_err & DAVINCI_I2C_STR_NACK)) {
    				w = davinci_i2c_read_reg(dev,
    							 DAVINCI_I2C_MDR_REG);
    				w |= DAVINCI_I2C_MDR_STP;
    				davinci_i2c_write_reg(dev,
    						      DAVINCI_I2C_MDR_REG, w);
    			}
    			complete(&dev->cmd_complete);
    			break;
    
    		case DAVINCI_I2C_IVR_RDR:
    			if (dev->buf_len) {
    				*dev->buf++ =
    				    davinci_i2c_read_reg(dev,
    							 DAVINCI_I2C_DRR_REG);
    				dev->buf_len--;
    				if (dev->buf_len)
    					continue;
    
    				davinci_i2c_write_reg(dev,
    					DAVINCI_I2C_STR_REG,
    					DAVINCI_I2C_IMR_RRDY);
    			} else {
    				/* signal can terminate transfer */
    				terminate_read(dev);
    			}
    			break;
    
    		case DAVINCI_I2C_IVR_XRDY:
    			if (dev->buf_len) {
    				davinci_i2c_write_reg(dev, DAVINCI_I2C_DXR_REG,
    						      *dev->buf++);
    				dev->buf_len--;
    				if (dev->buf_len)
    					continue;
    
    				w = davinci_i2c_read_reg(dev,
    							 DAVINCI_I2C_IMR_REG);
    				w &= ~DAVINCI_I2C_IMR_XRDY;
    				davinci_i2c_write_reg(dev,
    						      DAVINCI_I2C_IMR_REG,
    						      w);
    			} else {
    				/* signal can terminate transfer */
    				terminate_write(dev);
    			}
    			break;
    
    		case DAVINCI_I2C_IVR_SCD:
    			davinci_i2c_write_reg(dev,
    				DAVINCI_I2C_STR_REG, DAVINCI_I2C_STR_SCD);
    			complete(&dev->cmd_complete);
    			break;
    
    		case DAVINCI_I2C_IVR_AAS:
    			dev_dbg(dev->dev, "Address as slave interrupt\n");
    			break;
    
    		default:
    			dev_warn(dev->dev, "Unrecognized irq stat %d\n", stat);
    			break;
    		}
    	}
    
    	return count ? IRQ_HANDLED : IRQ_NONE;
    }
    
    #ifdef CONFIG_CPU_FREQ
    static int i2c_davinci_cpufreq_transition(struct notifier_block *nb,
    				     unsigned long val, void *data)
    {
    	struct davinci_i2c_dev *dev;
    
    	dev = container_of(nb, struct davinci_i2c_dev, freq_transition);
    	if (val == CPUFREQ_PRECHANGE) {
    		wait_for_completion(&dev->xfr_complete);
    		davinci_i2c_reset_ctrl(dev, 0);
    	} else if (val == CPUFREQ_POSTCHANGE) {
    		i2c_davinci_calc_clk_dividers(dev);
    		davinci_i2c_reset_ctrl(dev, 1);
    	}
    
    	return 0;
    }
    
    static inline int i2c_davinci_cpufreq_register(struct davinci_i2c_dev *dev)
    {
    	dev->freq_transition.notifier_call = i2c_davinci_cpufreq_transition;
    
    	return cpufreq_register_notifier(&dev->freq_transition,
    					 CPUFREQ_TRANSITION_NOTIFIER);
    }
    
    static inline void i2c_davinci_cpufreq_deregister(struct davinci_i2c_dev *dev)
    {
    	cpufreq_unregister_notifier(&dev->freq_transition,
    				    CPUFREQ_TRANSITION_NOTIFIER);
    }
    #else
    static inline int i2c_davinci_cpufreq_register(struct davinci_i2c_dev *dev)
    {
    	return 0;
    }
    
    static inline void i2c_davinci_cpufreq_deregister(struct davinci_i2c_dev *dev)
    {
    }
    #endif
    
    static struct i2c_algorithm i2c_davinci_algo = {
    	.master_xfer	= i2c_davinci_xfer,
    	.functionality	= i2c_davinci_func,
    };
    
    static const struct of_device_id davinci_i2c_of_match[] = {
    	{.compatible = "ti,davinci-i2c", },
    	{.compatible = "ti,keystone-i2c", },
    	{},
    };
    MODULE_DEVICE_TABLE(of, davinci_i2c_of_match);
    
    static int davinci_i2c_probe(struct platform_device *pdev)
    {
    	struct davinci_i2c_dev *dev;
    	struct i2c_adapter *adap;
    	struct resource *mem;
    	int r, irq;
    
    	irq = platform_get_irq(pdev, 0);
    	if (irq <= 0) {
    		if (!irq)
    			irq = -ENXIO;
    		if (irq != -EPROBE_DEFER)
    			dev_err(&pdev->dev,
    				"can't get irq resource ret=%d\n", irq);
    		return irq;
    	}
    
    	dev = devm_kzalloc(&pdev->dev, sizeof(struct davinci_i2c_dev),
    			GFP_KERNEL);
    	if (!dev) {
    		dev_err(&pdev->dev, "Memory allocation failed\n");
    		return -ENOMEM;
    	}
    
    	init_completion(&dev->cmd_complete);
    #ifdef CONFIG_CPU_FREQ
    	init_completion(&dev->xfr_complete);
    #endif
    	dev->dev = &pdev->dev;
    	dev->irq = irq;
    	dev->pdata = dev_get_platdata(&pdev->dev);
    	platform_set_drvdata(pdev, dev);
    
    	if (!dev->pdata && pdev->dev.of_node) {
    		u32 prop;
    
    		dev->pdata = devm_kzalloc(&pdev->dev,
    			sizeof(struct davinci_i2c_platform_data), GFP_KERNEL);
    		if (!dev->pdata)
    			return -ENOMEM;
    
    		memcpy(dev->pdata, &davinci_i2c_platform_data_default,
    			sizeof(struct davinci_i2c_platform_data));
    		if (!of_property_read_u32(pdev->dev.of_node, "clock-frequency",
    			&prop))
    			dev->pdata->bus_freq = prop / 1000;
    
    		dev->pdata->has_pfunc =
    			of_property_read_bool(pdev->dev.of_node,
    					      "ti,has-pfunc");
    	} else if (!dev->pdata) {
    		dev->pdata = &davinci_i2c_platform_data_default;
    	}
    
    	dev->clk = devm_clk_get(&pdev->dev, NULL);
    	if (IS_ERR(dev->clk))
    		return -ENODEV;
    	clk_prepare_enable(dev->clk);
    
    	mem = platform_get_resource(pdev, IORESOURCE_MEM, 0);
    	dev->base = devm_ioremap_resource(&pdev->dev, mem);
    	if (IS_ERR(dev->base)) {
    		r = PTR_ERR(dev->base);
    		goto err_unuse_clocks;
    	}
    
    	i2c_davinci_init(dev);
    
    	r = devm_request_irq(&pdev->dev, dev->irq, i2c_davinci_isr, 0,
    			pdev->name, dev);
    	if (r) {
    		dev_err(&pdev->dev, "failure requesting irq %i\n", dev->irq);
    		goto err_unuse_clocks;
    	}
    
    	r = i2c_davinci_cpufreq_register(dev);
    	if (r) {
    		dev_err(&pdev->dev, "failed to register cpufreq\n");
    		goto err_unuse_clocks;
    	}
    
    	adap = &dev->adapter;
    	i2c_set_adapdata(adap, dev);
    	adap->owner = THIS_MODULE;
    	adap->class = I2C_CLASS_DEPRECATED;
    	strlcpy(adap->name, "DaVinci I2C adapter", sizeof(adap->name));
    	adap->algo = &i2c_davinci_algo;
    	adap->dev.parent = &pdev->dev;
    	adap->timeout = DAVINCI_I2C_TIMEOUT;
    	adap->dev.of_node = pdev->dev.of_node;
    
    	if (dev->pdata->has_pfunc)
    		adap->bus_recovery_info = &davinci_i2c_scl_recovery_info;
    	else if (dev->pdata->scl_pin) {
    		adap->bus_recovery_info = &davinci_i2c_gpio_recovery_info;
    		adap->bus_recovery_info->scl_gpio = dev->pdata->scl_pin;
    		adap->bus_recovery_info->sda_gpio = dev->pdata->sda_pin;
    	}
    
    	adap->nr = pdev->id;
    	r = i2c_add_numbered_adapter(adap);
    	if (r) {
    		dev_err(&pdev->dev, "failure adding adapter\n");
    		goto err_unuse_clocks;
    	}
    
    	return 0;
    
    err_unuse_clocks:
    	clk_disable_unprepare(dev->clk);
    	dev->clk = NULL;
    	return r;
    }
    
    static int davinci_i2c_remove(struct platform_device *pdev)
    {
    	struct davinci_i2c_dev *dev = platform_get_drvdata(pdev);
    
    	i2c_davinci_cpufreq_deregister(dev);
    
    	i2c_del_adapter(&dev->adapter);
    
    	clk_disable_unprepare(dev->clk);
    	dev->clk = NULL;
    
    	davinci_i2c_write_reg(dev, DAVINCI_I2C_MDR_REG, 0);
    
    	return 0;
    }
    
    #ifdef CONFIG_PM
    static int davinci_i2c_suspend(struct device *dev)
    {
    	struct platform_device *pdev = to_platform_device(dev);
    	struct davinci_i2c_dev *i2c_dev = platform_get_drvdata(pdev);
    
    	/* put I2C into reset */
    	davinci_i2c_reset_ctrl(i2c_dev, 0);
    	clk_disable_unprepare(i2c_dev->clk);
    
    	return 0;
    }
    
    static int davinci_i2c_resume(struct device *dev)
    {
    	struct platform_device *pdev = to_platform_device(dev);
    	struct davinci_i2c_dev *i2c_dev = platform_get_drvdata(pdev);
    
    	clk_prepare_enable(i2c_dev->clk);
    	/* take I2C out of reset */
    	davinci_i2c_reset_ctrl(i2c_dev, 1);
    
    	return 0;
    }
    
    static const struct dev_pm_ops davinci_i2c_pm = {
    	.suspend        = davinci_i2c_suspend,
    	.resume         = davinci_i2c_resume,
    };
    
    #define davinci_i2c_pm_ops (&davinci_i2c_pm)
    #else
    #define davinci_i2c_pm_ops NULL
    #endif
    
    /* work with hotplug and coldplug */
    MODULE_ALIAS("platform:i2c_davinci");
    
    static struct platform_driver davinci_i2c_driver = {
    	.probe		= davinci_i2c_probe,
    	.remove		= davinci_i2c_remove,
    	.driver		= {
    		.name	= "i2c_davinci",
    		.pm	= davinci_i2c_pm_ops,
    		.of_match_table = davinci_i2c_of_match,
    	},
    };
    
    /* I2C may be needed to bring up other drivers */
    static int __init davinci_i2c_init_driver(void)
    {
    	return platform_driver_register(&davinci_i2c_driver);
    }
    subsys_initcall(davinci_i2c_init_driver);
    
    static void __exit davinci_i2c_exit_driver(void)
    {
    	platform_driver_unregister(&davinci_i2c_driver);
    }
    module_exit(davinci_i2c_exit_driver);
    
    MODULE_AUTHOR("Texas Instruments India");
    MODULE_DESCRIPTION("TI DaVinci I2C bus adapter");
    MODULE_LICENSE("GPL");
    

    see davinci_i2c_scl_prepare_recovery(), davinci_i2c_scl_unprepare_recovery(), i2c_davinci_wait_bus_not_busy, davinci_i2c_prepare_recovery(), davinci_i2c_unprepare_recovery(). 

    Also see i2c_generic_recovery() from i2c-core.c

    Hope this helps. 

    Best Regards, 
    Yordan

  • Well it might help sometime when I know that it is possible with TMS320C6672 and do not find RTOS or better OS-free chip specific templates to use SCL and SDA as GPIO.

    Right now my main concern and question is, if gpio wise access to SCL and SDA is possible with TMS320C6672 at all.

  • Meanwhile I took a brief look to the thread
    e2e.ti.com/.../2149364



    My current conclusions from this and other researcher are:

    1.) It is not possible to access SDA and SCL gpio wise for TMS320C6672

    2.) Harware designers should consider additional recovery logic like suggested in www.ti.com/.../sprugv3.pdf Figure A-4 (an interesting approach fro me is also www.analog.com/.../54305147357414AN686_0.pdf )

    3.) There may be a workaround implementing a bus recovery initiated from TMS320C667x without additional hardware using the loopback funktion of the I2C Module but this is not proven and would not help if an I2C eeprom is used as boot device.