Part Number: DRA626
Other Parts Discussed in Thread: TLV320AIC3106, PCF8575, TPS65910,
Tool/software: Linux
I am trying to change some flags for my / partition in /etc/fstab but they seem to not be taking affect.
Also I do not see in the /etc/fstab where the mmcblk mounts are.
Is there another area where I need to make these changes to have them take affect?
I tried this and a few derivations of it....
rootfs / auto auto,exec,relatime,sync,barrier=1,commit=1,data=ordered,data_err=abort,noatime 1 1
proc /proc proc exec,relatime,sync_barrier=1,commit=1,data=ordered,data_err=abort,noatime 0 0
devpts /dev/pts devpts mode=0620,gid=5 0 0
usbfs /proc/bus/usb usbfs defaults 0 0
tmpfs /var/volatile tmpfs defaults,size=16M 0 0
tmpfs /dev/shm tmpfs mode=0777 0 0
tmpfs /media/ram tmpfs defaults,size=16M 0 0
# uncomment this if your device has a SD/MMC/Transflash slot
#/dev/mmcblk0p1 /media/card auto defaults,sync,noauto 0 0
/dev/mmcblk0p2 /media/mmcblk0p2 auto defaults,data=ordered,sync,relatime
but anything I try results in this
root@c6a811x-evm:~# mount
rootfs on / type rootfs (rw)
/dev/root on / type ext3 (rw,relatime,errors=continue,user_xattr,acl,barrier=0,data=writeback)
devtmpfs on /dev type devtmpfs (rw,relatime,size=84880k,nr_inodes=21220,mode=755)
proc on /proc type proc (rw,noatime)
tmpfs on /mnt/.splash type tmpfs (rw,relatime,size=40k)
sysfs on /sys type sysfs (rw,relatime)
none on /dev type tmpfs (rw,relatime,size=1024k,nr_inodes=8192,mode=755)
/dev/mmcblk0p2 on /media/mmcblk0p2 type ext3 (rw,relatime,errors=continue,user_xattr,acl,barrier=0,data=writeback)
/dev/mmcblk0p1 on /media/mmcblk0p1 type vfat (rw,relatime,fmask=0022,dmask=0022,codepage=cp437,iocharset=iso8859-1,shortname=mixed,errors=remount-ro)
devpts on /dev/pts type devpts (rw,relatime,gid=5,mode=620)
usbfs on /proc/bus/usb type usbfs (rw,relatime)
tmpfs on /var/volatile type tmpfs (rw,relatime,size=16384k)
tmpfs on /dev/shm type tmpfs (rw,relatime,mode=777)
tmpfs on /media/ram type tmpfs (rw,relatime,size=16384k)