Part Number: DRA722
Tool/software: Linux
I met a problem , from the DRA72xx TRM,i get some discriptions like the following:
"the OCP2SCP_TIMING[9:7] DIVISIONRATIO bit field, with a valid range of 0x1 to 0x7,The OCP2SCP_TIMING[6:4] SYNC1 timing information is programmable in the range 0 to 7 clock cycles, and shows the acceptable delay between the enable and command availability on SCP. The value of OCP2SCP_TIMING[3:0] SYNC2 is also programmable in the range 1 to 15 clock cycles, measured from the moment the command is available on SCP until data is accessible."
I want to know is there any effects if we set different value to OCP2SCP_TIMING register?