This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux: Load bare metal DSP example using csl library

Other Parts Discussed in Thread: AM5728

Tool/software: Linux

Hi TI Team!

In one of our projects we will use an AM5728 SOC which has 2 C66x DSPs. Can someone explain which steps are necessary to:

1. Create a C66x baremetal application using only the chip support library from the MCSDK package.

2. Load this baremetal binary to one of the C66x processors using the A15 as master, which is running Linux.

I've found tons of TI-RTOS examples for the C66x and for the A15, but none of the examples matches my specific setup.

Thanks, regards,
Franz