Part Number: AM5728
Hi,
I have one question regarding AM5728 POH data.
According to Table5-3 of AM5728DS(SPRS953B), POH is specified in it.
But this table is written only POH(Lifetime) when junction temp(Tj) are 100degC and 105degC.
My customer would like to know the POH when other Junction temp.
According to note(1) of Table5-3,the below sentence is written.
(1) Unless specified in Table 5-3, all voltage domains and operating conditions are supported in the device at the noted temperatures.
Does this mean that POH covers if Junction temp is lower than specified temp in Table5-3
For example,
Extended device, OPP_HIGH, HDMI-not used, Junction temp is 95degC ----> This POH is 55K?
Extended device, OPP_HIGH, HDMI-used, Junction temp is 103degC ----> This POH is 45K?
Is my understanding right? Please let me know.
I appreciate your quick reply.
Best regards,
Michi