Hi,
I am trying to capture a RAW image (bayer pattern) with the DM6437 and am getting some image vertical drifting issues. I attached an example of the kind of image I get after some time of displaying.
Note that the drift in time is not regular (actually, it can correctly capture during several seconds, and then slightly drift and get back to a stable vertically shifted image for some other seconds...)
Here is my current configuration:
- Bayer input image
- CCDC sends the image to the previewer via the video port
- Previewer writes image in DDR
- Resizer takes image from DDR and writes it back to it
- Image is then transferred via Ethernet to a PC for display
- I am using TI video drivers
Note that I observe that drift at the Previewer output.
Please let me know if you can give me a hint where to look at.
Thanks
Franck