Part Number: AM3352
Other Parts Discussed in Thread: AM3352
Hi,
Am3352 based CPU system is used on custom design. It is very similar to AM335X reference design provided by TI. Recently I have met some problems when doing iperf test. PC functions as iperf server. Am3352 based CPU system functions as client. By the way I am running linux system based on SDK08.00.00.00. After some times running this test, the load of CPU is 100%. Then we can see throughput of iperf sharply comes down.
i do not think this is caused by low performance of AM3352. Maybe I miss something. Any advice will be appreciated. By the way I am using default setting about system control in kernel.
Best Regards
Yang