This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: GPMC to HPI connection issue

Part Number: AM3352

Hi Sir 

we connect GPMC intetface of AM3352 with HPI interface of C6748 and implement the SW code.

we also set internal pullup for AM3352 WAIT0 and DSP6748 UHPI_HRDY

there is one issue about the pullup resisor of GMPC wait0 pin.

If wait0 pullup resisor is 33ohm , the communication is succeed. 

If wait0 pullup resisor is 4.7kohm , the communication is failed. 

what is the suitable pull resistor value and what is the GPMC wait0 input impedence of AM3352 ? 

thanks for reply

BR

Yimin