Part Number: AM4379
Tool/software: Linux
Hi, Everyone
I have a question about RTLinux for AM437x using AM437xSK.
My customer develop for EtherCAT Master using RTLinux.
They want to change interrupt proority.
They see 2 Ethernet interrupt using "cat /proc/interrupts"command.
==
173: 0 WUGEN 41 Level 4a100000.ethernet
174: 0 WUGEN 42 Level 4a100000.ethernet
==
and They looked for SoftIrqHandler of Ethernet using "ps –A | grep irq" command.
==
PID TTY TIME CMD
3 ? 00:00:00 ksoftirqd/0
19 ? 00:00:00 irq/20-l3-dbg-i
20 ? 00:00:00 irq/21-l3-app-i
21 ? 00:00:00 irq/36-44e07000
23 ? 00:00:00 irq/69-4804c000
24 ? 00:00:00 irq/102-4832000
25 ? 00:00:00 irq/135-4832200
30 ? 00:00:00 irq/24-49000000
31 ? 00:00:00 irq/26-49000000
54 ? 00:00:00 irq/180-4808000
68 ? 00:00:00 irq/171-mmc0
70 ? 00:00:00 irq/186-OMAP DI
72 ? 00:00:00 irq/168-44e0b00
73 ? 00:00:00 irq/219-tps6521
74 ? 00:00:00 irq/169-4802a00
75 ? 00:00:00 irq/170-mmc1
76 ? 00:00:00 irq/43-48060000
261 ? 00:00:00 irq/23-wkup_m3_
262 ? 00:00:00 irq/32-wkup_m3
300 ? 00:00:00 irq/33-rtc0
307 ? 00:00:00 irq/34-rtc0
343 ? 00:00:00 irq/179-4831000
351 ? 00:00:00 irq/184-vpfe_ca
354 ? 00:00:00 irq/181-dwc3-om
355 ? 00:00:00 irq/182-dwc3-om
361 ? 00:00:00 irq/68-edt-ft53
374 ? 00:00:00 irq/176-5310000
451 ? 00:00:00 irq/141-matrix-
453 ? 00:00:00 irq/142-matrix-
620 ? 00:00:00 irq/181-dwc3-ot
621 ? 00:00:00 irq/181-s-dwc3-
624 ? 00:00:00 irq/222-xhci-hc
733 ? 00:00:00 irq/30-44e09000
==
but We do not find Ethernet interrupt in SoftIrqHandler.
If we find, I guess we can change priority. but we do not see this interrupt.
Can you tell me how to change Ethernet interrupt priority ?
Best Regards
Hiroyasu