Other Parts Discussed in Thread: AM5728
Tool/software: TI-RTOS
Hello,
I have a customer who is trying to create a bootable SD card for an application that she is writing. The TI-RTOS application runs on a custom AM572X based board and we have verified that it runs through JTAG. However for the actual use case the customer would like to create an SD card to host the application so that no jtag connection is needed.
We have successfully used the pdkAppImageCreate.bat script to generate an "app" image from the compiled .out file. I have tried using both release and debug targets as the source of the binary to no avail.
I have rebuit PDK so that the MLO reflects the changes to the board files we made as necessary. I have tried multiple bootable FAT partitioned SD cards and none of them appear to be working.
Here is the process we are using for generating these SD cards:
- Create bootable FAT partition on SD card as the first partition
- Use pdkAppImageCreate.bat to generate an "app" file
- Copy MLO from boot\sbl\binary\evmAM572x\mmcsd\bin to SD card
- Copy "app" file to SD card
- Boot board (boot order includes mmcsd and there is nothing else that's bootable on the system)
Is there something we are missing in this whole process?
Regards,
Munan