This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: GPIO interrupts

Part Number: AM5728

Dear all,

I have a question regarding AM572x GPIO controller. By reading the reference manual i observed that GPIO instance has two Interrupt lines which can be independently configured. But by looking at the Edge Triggering registers, Its not available for both the instances. So I am bit confused if we enabled both the line would Edge Trigger not be independent for both of them. If no what exactly is the use case of having two interrupt lines. For example: If i want to configure GPIO 1 to for independently for both the "Rising Edge" and "Falling Edge", Would it be possible ? Thanks in advance.

Best Regards,

Hamza.