This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: GPIO load capacitance

Part Number: AM3352

Hi,

What could be the maximum load capacitance that AM335x GPIO could support?
I understand this won't be mentioned in the datasheet.

In our application below pins need to be connected to a high capacitance devices,
will such high load capacitance destroy the GPIO?

M18(MDC) pin -> 2200pF load
U17(GPMC_WPn) pin -> 120pF load

As per the below E2E, it seems the AIN terminals was designed with the capability of
driving high capacitance loads, will it be similar with other pins (above) also?
e2e.ti.com/.../1144614

Best Regards
Kummi