Part Number: OMAP-L138
I run the app_spi_flash on CCS. The Console window has a "Enter the app image load address (in hex):" request, so I can see where that address is.
[C674X_0] Starting OMAP-L138 SPIWriter.
Will you be writing a UBL image? (Y or y)
y
Enter the binary AIS UBL file name (enter 'none' to skip):
none
DONE.
Enter the application file name (enter 'none' to skip):
ECHO_Secure.ais
INFO: File read complete.
Enter the app image load address (in hex):
0x..........
Enter the app image entry point address (in hex):
0xc1080000