Part Number: AM5716
Tool/software: Linux
Hello,
We're debugging the AM5716 custom board with PSDK Linux v03.01.00.06. We have a problem with simultaneous use of USB1 and PCIE2.
We use USB1 as USB2.0 Host using USB2PHY1.
AM571x TRM (SPRUHZ7E) : Figure 24-138. USB1 Highlight
We use PCIE2 as a port of PCIe using USB3_PHY. We also use PCIE1 as another port of PCIe. Each of the opposite devices of PCIe ports is a PCIe-Ethernet Switch.
Figure 26-18. PCIe PHY Subsystem Block Diagram
When I try to use USB1 as USB2.0 Host and PCIE2 simultaneously, a kernel crash occurs during boot. When I don't initialize PCIE at all or use only PCIE1 (x1 mode), it boots normally and works fine. I attached the boot log added some NOTEs, please give me some advice.
Regards,
Kazu