This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/BEAGLEBN: beaglebone green wireless

Part Number: BEAGLEBN

Tool/software: Linux

I'm trying to get 802.11s mesh networking running on the "beaglebone green wireless (AM335x)" by the step on WL18xx System Build Scripts (processors.wiki.ti.com/.../WL18xx_System_Build_Scripts).

1. First, I downloaded "ti-processor-sdk-linux-am335x-evm-03.02.00.05" to follow the setting steps in the webside, but it didn't work.

After   "./build_wl18xx.sh update R8.7", the console appeared "your kernel headers are incompletee/not installed" . (Please refer the next picture.)

I tried to use the command "apt-get install build-essential linux-headers-$(uname -r) ", but it did not work.

 

2. Then I download "ti-sdk-am335x-evm-07.00.00.00-Linux-x86" to follow the setting steps.

After   "./build_wl18xx.sh update R8.7", the console appeared 

"Kernel configuration is invalid. include/generated/autoconf.h or include/config/auto.conf are missing."(Please refer the next picture.)

I tried to use the command " sudo apt-get install autoconf", but it did not work.


Should I use "ti-processor-sdk-linux-am335x-evm-03.02.00.05" or "ti-sdk-am335x-evm-07.00.00.00-Linux-x86"?

And how can I fix the problems to get 802.11s mesh networking running on the "beaglebone green wireless (AM335x)" ?

Please help to fix the problem, thanks.