This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Starterware/STARTERWARE-SITARA: eqep module problem

Part Number: STARTERWARE-SITARA


Tool/software: Starterware

Hey everyone,

i am trying to set up an eqep driver for my beaglebone white. I believe that i have enabled the power and clock domain that are required.
My next step is to pass (with the following piece of code) the desired values to the appropriate registers.

HWREG(SOC_EQEP_1_REGS+EQEP_QPOSCNT) = 0x00000000;
HWREG(SOC_EQEP_1_REGS+EQEP_QPOSINIT) = 0x000A;
HWREG(SOC_EQEP_1_REGS+EQEP_QPOSMAX) = 0xFFFF;
HWREG(SOC_EQEP_1_REGS+EQEP_QDECCTL) = 0x0800;
HWREG(SOC_EQEP_1_REGS+EQEP_QEPCTL) = 0x12B8;
HWREG(SOC_EQEP_1_REGS+EQEP_QEINT) = 0x0000;
HWREG(SOC_EQEP_1_REGS+EQEP_QFLG) = 0x0000;
HWREG(SOC_EQEP_1_REGS+EQEP_QCLR) = 0x0000;

well everything seems to work as wanted except for when the code reaches the value of EQEP_QEPCTL register...
i mean the program seems to stuck there, unable to move on and pass the other values to the other registers..
The same happens if i comment out the line regarding QEPCTL register but i leave those lines regarding QEINT and QFLG registers..
My guess is that the eqep module is not properly initialized or that the value i give to those registers are not acceptable(but i have tried other values with the same result)..

So could anyone help or point out the proper (and necessary) way to initialize the eqep module?

Thanks in advance!