Part Number: TMS320C6678
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320C6678
Hi Daisuke,
The hardware design guide clearly states:
"All HyperLink clock and data pins (MCMRXFLCLK, MCMRXFLDAT, MCMTXFLCLK, MCMTXFLDAT, MCMRXPMCLK, MCMRXPMDAT,
MCMTXPMCLK, MCMTXPMDAT) can be left floating when the entire HyperLink peripheral is not used. Each unused HyperLink clock and data pin will be pulled low when not in use through internal pull-down resistors. "
"If the HyperLink interface is not being used, the peripheral should be disabled in the MMR."
"If the HyperLink interface is not required, the HyperLink regulator power pin (VDDR1_MCM) must still be connected to the correct supply rail with the appropriate
decoupling capacitance applied. The EMI/Noise filter is not required when this interface is not used."
"If unused, the primary HyperLink clock input must be configured as indicated in Section 3.3, Figure 13. Pull-up must be to the CVDD core supply."
So to answer your question, if you DO NOT use the entire Hyperlink, then you should leave all clock and data pins unconnected with the internal pull-down resistors enabled. The power should still be connected. The clock must be configured, as described in the Hardware Design Guide.
Best Regards,
Yordan
For all other SerDes interface (SGMII, SRIO, PCIe), "Hardware Design Guide for KeyStone Devices (Rev. C)" (SPRABI2C) describes that those pins must be left floating.