This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/LAUNCHXL-CC1310: CC1310 output 24MHz crystal

Part Number: LAUNCHXL-CC1310
Other Parts Discussed in Thread: CC1310

Tool/software: TI-RTOS

CC1310 LaunchPand external 24MHz crystal oscillator and external 32KHz crystal output? If yes, which IO port output?

  • Hi,

    You cannot output the 24 MHz oscillator on a pin. If you want to measure the clock accuracy, you can look at the RF carrier with a spectrum analyzer. The relative frequency offset is the same.

    To output the 32 kHz clock on an IO, see the Technical Reference Manual (www.ti.com/lit/pdf/swcu117) section 11.3.3.

    Cheers,
    Fredrik